![]() |
![]() |
ECDHCC26X1 Object. More...
#include <ECDHCC26X1.h>
Data Fields | |
bool | isOpen |
ECDH_CallbackFxn | callbackFxn |
ECDH_ReturnBehavior | returnBehavior |
ECC_State | eccState |
uint32_t | eccWorkZone [171] |
ECDHCC26X1 Object.
The application must not access any member variables of this structure!
bool ECDHCC26X1_Object::isOpen |
ECDH_CallbackFxn ECDHCC26X1_Object::callbackFxn |
ECDH_ReturnBehavior ECDHCC26X1_Object::returnBehavior |
ECC_State ECDHCC26X1_Object::eccState |
uint32_t ECDHCC26X1_Object::eccWorkZone[171] |