![]() |
![]() |
DACCC26XX Object. More...
#include <DACCC26X2.h>
Data Fields | |
bool | isEnabled |
PIN_State | pinState |
PIN_Handle | pinHandle |
bool | isOpen |
uint32_t | currCode |
uint32_t | dacOutputMin |
uint32_t | dacOutputMax |
DACCC26XX Object.
The application must not access any member variables of this structure!
bool DACCC26XX_Object::isEnabled |
< Flag to determine current state of the DAC's output Pin state object
PIN_State DACCC26XX_Object::pinState |
Pin handle
PIN_Handle DACCC26XX_Object::pinHandle |
Flag if the instance is in use
bool DACCC26XX_Object::isOpen |
Current DAC code set
uint32_t DACCC26XX_Object::currCode |
Minimum DAC output in uV
uint32_t DACCC26XX_Object::dacOutputMin |
Maximum DAC output in uV
uint32_t DACCC26XX_Object::dacOutputMax |