TI Logo
SimpleLink™ CC13x2 / CC26x2 SDK BLE5-Stack User's Guide
2.02.02.00
  • Disclaimer
  • Introduction to the SimpleLink CC13x2 / 26x2 SDK
  • TI BLE5-Stack Quick Start
  • The CC13x2 or CC26x2 SDK Platform
  • TI-RTOS (RTOS Kernel) Overview
  • Application
  • BLE5-Stack
  • Developing a Custom Application
  • Running the SDK on Custom Hardware
  • Coexistence
  • RTLS Toolbox
  • Bluetooth Mesh
  • Micro BLE Stack
  • Sensor Controller
  • Debugging
  • Memory overview
  • Network Processor Interface (NPI)
  • Over-the-Air Download (OAD)
  • System Configuration Tool (SysConfig)
    • Get started with SysConfig
    • Configure The Board Files with SysConfig
    • Migrating Board Variant
    • BLE5-Stack SysConfig Features
    • Disable SysConfig
  • EnergyTrace User Guide
  • Porting Guide and Migration Guides
  • API References
  • Terms and Definitions




SimpleLink™ CC13x2 / CC26x2 SDK BLE5-Stack User's Guide
  • »
  • System Configuration Tool (SysConfig)

System Configuration Tool (SysConfig)¶

SysConfig is a graphical tool for configuring your SimpleLink SDK project. To set up SysConfig please see the section Get started with SysConfig.

  • Get started with SysConfig
    • Using Stand-alone SysConfig
    • Using SysConfig with IAR Workbench
    • Using SysConfig as a Plug-In to CCS
    • Viewing SysConfig Output
  • Configure The Board Files with SysConfig
  • Migrating Board Variant
  • BLE5-Stack SysConfig Features
    • Checking if SysConfig is used for BLE
    • Additional Configuration Categories
  • Disable SysConfig
    • First Method: Stop SysConfig From Running
    • Second Method: Exclude SysConfig From Build
Next Previous

2010-2020, Texas Instruments, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale