This module implements the RTLS Services APIs.
More...
|
bStatus_t | RTLSSrv_CLCteTransmitEnable (uint8 advHandle, uint8 enable) |
|
bStatus_t | RTLSSrv_init (uint8_t numOfRTLSConns) |
|
PIN_Handle | RTLSSrv_initAntArray (uint8_t mainAntenna) |
|
bStatus_t | RTLSSrv_processHciEvent (uint16_t hciEvt, uint16_t hciEvtSz, uint8_t *pEvtData) |
|
bStatus_t | RTLSSrv_readAntennaInformationCmd (void) |
|
bStatus_t | RTLSSrv_register (pfnAppEventHandlerCB_t pCB) |
|
bStatus_t | RTLSSrv_setCLCteSamplingEnableCmd (uint16_t syncHandle, uint8_t enable, uint8_t slotDuration, uint8_t maxSampleCte, uint8_t numAnt, uint8_t pAntPattern[]) |
|
bStatus_t | RTLSSrv_SetCLCteTransmitParams (uint8 advHandle, uint8 cteLength, uint8 cteType, uint8 cteCount, uint8 switchLen, uint8 *pAntenna) |
|
bStatus_t | RTLSSrv_setConnCteReceiveParams (uint16_t connHandle, uint8_t samplingEnable, uint8_t slotDurations, uint8_t numAnt, uint8_t antArray[]) |
|
bStatus_t | RTLSSrv_setConnCteRequestEnableCmd (uint16_t connHandle, uint8_t enable, uint16_t interval, uint8_t length, uint8_t type) |
|
bStatus_t | RTLSSrv_setConnCteResponseEnableCmd (uint16_t connHandle, uint8_t enable) |
|
bStatus_t | RTLSSrv_setConnCteTransmitParams (uint16_t connHandle, uint8_t types, uint8_t length, uint8_t antArray[]) |
|
bStatus_t | RTLSSrv_setCteSampleAccuracy (uint16_t handle, uint8_t sampleRate1M, uint8_t sampleSize1M, uint8_t sampleRate2M, uint8_t sampleSize2M, uint8_t sampleCtrl) |
|
This module implements the RTLS Services APIs.
§ RTLSSrv_CLCteTransmitEnable()
bStatus_t RTLSSrv_CLCteTransmitEnable |
( |
uint8 |
advHandle, |
|
|
uint8 |
enable |
|
) |
| |
RTLSSrv_CLCteTransmitEnable
Used to request the advertiser to enable or disable the periodic advertising for the advertising set
/ref did_214342976
- Parameters
-
advHandle | - Used to identify a periodic advertising train |
enable | - 0x00 - Periodic advertising is disabled (default)
- 0x01 - Periodic advertising is enabled
|
- Returns
- SUCCESS, RTLSSRV_BAD_PARAMETER, RTLSSRV_COMMAND_DISALLOWED
§ RTLSSrv_init()
bStatus_t RTLSSrv_init |
( |
uint8_t |
numOfRTLSConns | ) |
|
Initialize RTLSSrv module
- Parameters
-
numOfRTLSConns | - number of connections that RTLS Srv is required to support |
- Returns
- SUCCESS/FAILURE
§ RTLSSrv_initAntArray()
PIN_Handle RTLSSrv_initAntArray |
( |
uint8_t |
mainAntenna | ) |
|
Initialize antenna array To initialize a single pin, use array of length 1
- Parameters
-
mainAntenna | - Antenna ID to be used as main receiving antenna |
- Returns
- PIN_Handle - handle for initialized pins
§ RTLSSrv_processHciEvent()
bStatus_t RTLSSrv_processHciEvent |
( |
uint16_t |
hciEvt, |
|
|
uint16_t |
hciEvtSz, |
|
|
uint8_t * |
pEvtData |
|
) |
| |
RTLSSrv_processHciEvent
This is the HCI event handler for RTLSSrv module Any HCI event related to RTLS should pass through this API
- Parameters
-
- Returns
- TRUE = success, FALSE = failure
§ RTLSSrv_readAntennaInformationCmd()
bStatus_t RTLSSrv_readAntennaInformationCmd |
( |
void |
| ) |
|
§ RTLSSrv_register()
Register callback functions with RTLS Services
- Parameters
-
pCB | pointer to callback function structure |
- Returns
- SUCCESS/FAILURE
§ RTLSSrv_setCLCteSamplingEnableCmd()
bStatus_t RTLSSrv_setCLCteSamplingEnableCmd |
( |
uint16_t |
syncHandle, |
|
|
uint8_t |
enable, |
|
|
uint8_t |
slotDuration, |
|
|
uint8_t |
maxSampleCte, |
|
|
uint8_t |
numAnt, |
|
|
uint8_t |
pAntPattern[] |
|
) |
| |
RTLSSrv_setCLCteSamplingEnableCmd
Request the Controller to enable or disable capturing IQ samples from the CTE of periodic advertising packets in the periodic advertising train identified by the syncHandle parameter.
/ref did_214342976
- Parameters
-
syncHandle | - Handle identifying the periodic advertising train (Range: 0x0000 to 0x0EFF) |
enable | - 0x00 - Disable CTE sampling
- 0x01 - Enable CTE sampling
|
slotDuration | - Switching and sampling slots in 1 us or 2 us each (1 or 2). |
maxSampleCte | - 0 - Sample and report all available CTEs
1-16 - Max number of CTEs to sample and report in each periodic event |
numAnt | - Number of items in Antenna array (relevant to AoA only) |
pAntPattern | - Pointer to Antenna array (relevant to AoA only) |
- Returns
- SUCCESS, RTLSSRV_COMMAND_DISALLOWED, RTLSSRV_BAD_PARAMETER RTLSSRV_UNKNOWN_ADVERTISING_IDENTIFIER
§ RTLSSrv_SetCLCteTransmitParams()
bStatus_t RTLSSrv_SetCLCteTransmitParams |
( |
uint8 |
advHandle, |
|
|
uint8 |
cteLength, |
|
|
uint8 |
cteType, |
|
|
uint8 |
cteCount, |
|
|
uint8 |
switchLen, |
|
|
uint8 * |
pAntenna |
|
) |
| |
RTLSSrv_SetCLCteTransmitParams
Used to request the advertiser to enable or disable the periodic advertising for the advertising set
/ref did_214342976
- Parameters
-
advHandle | - Used to identify a periodic advertising train |
cteLength | - CTE length in 8 us units. |
cteType | - 0x00 - AoA CTE
- 0x01 - AoD CTE with 1 us slots.
- 0x02 - AoD CTE with 2 us slots.
|
cteCount | - The number of CTE to transmit in each periodic advertising interval. Range: 0x01-0x10 |
switchLen | - The number of Antenna IDs in the pattern. Range: 0x02-0x4B. |
pAntenna | - list of Antenna IDs in the pattern. |
- Returns
- SUCCESS, RTLSSRV_COMMAND_DISALLOWED, RTLSSRV_FEATURE_NOT_SUPPORTED, RTLSSRV_BAD_PARAMETER
§ RTLSSrv_setConnCteReceiveParams()
bStatus_t RTLSSrv_setConnCteReceiveParams |
( |
uint16_t |
connHandle, |
|
|
uint8_t |
samplingEnable, |
|
|
uint8_t |
slotDurations, |
|
|
uint8_t |
numAnt, |
|
|
uint8_t |
antArray[] |
|
) |
| |
Note: RTLSSrv_initAntArray must be called before calling this functions In order to not limit users GPIO configuration, it is the users responsibility to either call RTLSSrv_initAntArray or to initialize GPIO's in another manner
Used to:
- Enable or disable sampling received Constant Tone Extension fields on a connection
- Configure the antenna switching pattern
- Configure switching and sampling slot durations to be used
- Parameters
-
connHandle | - Connection handle |
samplingEnable | - Sample CTE on a connection and report the samples to the User Application (0 or 1) |
slotDurations | - Switching and sampling slots in 1 μs or 2 μs each (1 or 2) |
numAnt | - The number of Antenna IDs in the pattern (2 to 75) |
antArray | - List of Antenna IDs in the pattern |
- Returns
- bStatus_t - command was acked, async return status in case of an error provided by RTLS_ERROR_EVT
§ RTLSSrv_setConnCteRequestEnableCmd()
bStatus_t RTLSSrv_setConnCteRequestEnableCmd |
( |
uint16_t |
connHandle, |
|
|
uint8_t |
enable, |
|
|
uint16_t |
interval, |
|
|
uint8_t |
length, |
|
|
uint8_t |
type |
|
) |
| |
Start or stop initiating the CTE Request procedure on a connection Note that the API enables periodically requesting CTE by using the 'interval' parameter
- Parameters
-
connHandle | - Connection handle |
enable | - Enable or disable CTE Request for a connection (1 or 0) |
interval | - Requested interval for initiating the CTE Request procedure in number of connection events (1 to 0xFFFF).
1 means the next CTE Request procedure is initiated at the connection interval following the completion of a previous CTE Request procedure.
The first CTE Request procedure is sent as soon as possible no matter the value set for this parameter. |
length | - Min length of the CTE being requested in 8 μs units (2 to 20) |
type | - Requested CTE type (0 - AoA, 1 - AoD with 1μs slots, 2 - AoD with 2μs slots) |
- Returns
- bStatus_t - command was acked, async return status in case of an error provided by RTLS_ERROR_EVT
§ RTLSSrv_setConnCteResponseEnableCmd()
bStatus_t RTLSSrv_setConnCteResponseEnableCmd |
( |
uint16_t |
connHandle, |
|
|
uint8_t |
enable |
|
) |
| |
Enable responding to CTE requests
- Parameters
-
connHandle | - Connection handle |
enable | - Enable or disable CTE Response for a connection (1 or 0) |
- Returns
- bStatus_t - command was acked, async return status in case of an error provided by RTLS_ERROR_EVT
§ RTLSSrv_setConnCteTransmitParams()
bStatus_t RTLSSrv_setConnCteTransmitParams |
( |
uint16_t |
connHandle, |
|
|
uint8_t |
types, |
|
|
uint8_t |
length, |
|
|
uint8_t |
antArray[] |
|
) |
| |
Used to:
- Set the antenna switching pattern
- Set permitted Constant Tone Extension types used for transmitting Constant Tone Extensions requested by the peer device on a connection
- Parameters
-
connHandle | - Connection handle |
types | - CTE types (0 - Allow AoA CTE Response) |
length | - The number of Antenna IDs in the pattern (2 to 75) |
antArray | - List of Antenna IDs in the pattern |
- Returns
- bStatus_t - command was acked, async return status in case of an error provided by RTLS_ERROR_EVT
§ RTLSSrv_setCteSampleAccuracy()
bStatus_t RTLSSrv_setCteSampleAccuracy |
( |
uint16_t |
handle, |
|
|
uint8_t |
sampleRate1M, |
|
|
uint8_t |
sampleSize1M, |
|
|
uint8_t |
sampleRate2M, |
|
|
uint8_t |
sampleSize2M, |
|
|
uint8_t |
sampleCtrl |
|
) |
| |
Set CTE sampling accuracy
- Parameters
-
handle | Connection/sync handle. |
sampleRate1M | sample rate for PHY 1M range : 1 - least accuracy (as in 5.1 spec) to 4 - most accuracy |
sampleSize1M | sample size for PHY 1M range : 1 - 8 bits (as in 5.1 spec) or 2 - 16 bits (more accurate) |
sampleRate2M | sample rate for PHY 2M range : 1 - least accuracy (as in 5.1 spec) to 4 - most accuracy |
sampleSize2M | sample size for PHY 2M range : 1 - 8 bits (as in 5.1 spec) or 2 - 16 bits (more accurate) |
sampleCtrl | - sample control flags range : range : bit0=0 - Default filtering, bit0=1 - RAW_RF(no filtering), , bit1..7=0 - spare |
- Returns
- bStatus_t - command was acked, async return status in case of an error provided by RTLS_ERROR_EVT