Z-Stack 3.6.0+ to Z-Stack 4.3.0¶
This section will describe a way to migrate a projects Z-Stack 3.6.0 and later to a Z-Stack 4.3.0 project.
Note
Z-Stack 3.6.0 is the last 3.x version, the next being Z-Stack 4.1.0 and since then following the same SimpleLink CC13x2 / 26x2 SDK version naming convention.
For this guide, zc_light from Z-Stack 3.6.0 will be compared with Z-Stack 4.3.0. New features and updates that have occurred in between include:
- Project pre-definition changes
- Renaming of several ZCL definitions
- Revised callbacks and API names/parameters
- LED handling
The recommended approach is to start with a Z-Stack 4.3.0 project that contains the same base application as the porting target project and merge any custom functionality.
- Choose a Z-Stack 4.3.0 example project that contains your target project’s base functionality. For reference and use in this example, zc_light from C:\ti\simplelink_cc13x2_26x2_sdk_x_xx_xx_xx\examples\rtos\CC13x2 or CC26x2_LAUNCHXL\zstack is chosen as a starting point.
- Multiple application predefinitions have changed, including (but not limited to)
USE_ZCL_SAMPLEAPP_UItoCUI_DISABLEandOTA_CLIENTtoOTA_CLIENT_INTEGRATED. The list of current preprocessor definitions are available in Application Preprocessor Configuration and developers must take caution to modify their project settings and application files accordingly. For example, instances of#ifdef USE_ZCL_SAMPLEAPP_UIshould becomeifndef CUI_DISABLEinzcl_sample*.[c/h]. - As SysConfig has been upgraded to version 1.6.0, developers must modify their
Z-Stack settings (and thus the definitions generated for
ti_zstack_config.h) in the new.syscfgfile from the Z-Stack 4.3.0 project. Refer to the directions in Zigbee Configuration for more information. - Several ZCL files inside C:\ti\simplelink_cc13x2_26x2_sdk_x_xx_xx_xx\source\ti\zstack\stack\zcl have renamed
definitions for cluster IDs, attributes, and commands. For example,
ZCL_CLUSTER_ID_GEN_BASICfromzcl.his nowZCL_CLUSTER_ID_GENERAL_BASIC. Several changes have been made to other commonzcl*.hfiles includingzcl_general.handzcl_ha.h, among others. Affected definitions range fromZCL_*,COMMAND_*,ATTRID_*, and more. Developers must be sure to update thezcl_sample*_data.candzcl_sample*.cfiles accordingly for consistency. Other clusters, attributes, or simple descriptors which were added or altered in the previous Z-Stack project should also be migrated accordingly.
The following items specifically concern zcl_samplelight.c:
DMM functionality for related projects has been modified slightly, thus instances of
if USE_DMMare replaced with#if defined(USE_DMM) && defined(BLE_START).static void zclSampleLight_LevelControlMoveToClosestFrequencyCB( zclLCMoveFreq_t *pCmd );has been added and is placed in thezclGeneral_AppCallbacks_t zclSampleLight_CmdCallbackstable:static zclGeneral_AppCallbacks_t zclSampleLight_CmdCallbacks = { ... #ifdef ZCL_LEVEL_CTRL zclSampleLight_LevelControlMoveToLevelCB, // Level Control Move to Level command zclSampleLight_LevelControlMoveCB, // Level Control Move command zclSampleLight_LevelControlStepCB, // Level Control Step command zclSampleLight_LevelControlStopCB, // Level Control Stop command zclSampleLight_LevelControlMoveToClosestFrequencyCB, // Level Control Stop command #endif ... };
Also,
zclSampleLight_LevelControlStopCBnow has parameterzclLCStop_t *pCmdinstead ofvoid.Key and button handling have been modified:
#include <ti/drivers/apps/Button.h> #include <ti/drivers/apps/LED.h> ... ##ifndef CUI_DISABLE CONST char zclSampleLight_appStr[] = APP_TITLE_STR; CUI_clientHandle_t gCuiHandle; static LED_Handle gRedLedHandle; static uint32_t gSampleLightInfoLine; #endif ... #ifndef CUI_DISABLE static void zclSampleLight_processKey(uint8_t key, Button_EventMask buttonEvents); static void zclSampleLight_RemoveAppNvmData(void); static void zclSampleLight_InitializeStatusLine(CUI_clientHandle_t gCuiHandle); static void zclSampleLight_UpdateStatusLine(void); #endif ... //Request the Red LED for App LED_Params ledParams; LED_Params_init(&ledParams); gRedLedHandle = LED_open(CONFIG_LED_RED, &ledParams); //Initialize the sampleLight UI status line zclSampleLight_InitializeStatusLine(gCuiHandle); ... static void zclSampleLight_UpdateLedState(void) { #ifndef CUI_DISABLE // set the LED1 based on light (on or off) if ( LIGHT_ON == zclSampleLight_getOnOffAttribute()) { #ifdef ZCL_LEVEL_CTRL uint8_t lightLevel = zclSampleLight_getCurrentLevelAttribute(); // lightLevel is a value from 0-255. We must map this to a percentage (0-100%) LED_stopBlinking(gRedLedHandle); LED_setOn(gRedLedHandle, (lightLevel * 100) / 255); #else LED_stopBlinking(gRedLedHandle); LED_setOn(gRedLedHandle, LED_BRIGHTNESS_MAX); #endif } else { LED_stopBlinking(gRedLedHandle); LED_setOff(gRedLedHandle); } #endif } ... static void zclSampleLight_processKey(uint8_t key, Button_EventMask buttonEvents) { if (buttonEvents & Button_EV_CLICKED) { if(key == CONFIG_BTN_LEFT) { zstack_bdbStartCommissioningReq_t zstack_bdbStartCommissioningReq; zstack_bdbStartCommissioningReq.commissioning_mode = zclSampleLight_BdbCommissioningModes; Zstackapi_bdbStartCommissioningReq(appServiceTaskId, &zstack_bdbStartCommissioningReq); } if(key == CONFIG_BTN_RIGHT) { } } }
The
CUI_led*APIs are no longer used.zclport_registerZclHandleExternalnow includes an endpoint as the first parameter,zclport_registerZclHandleExternal(SAMPLELIGHT_ENDPOINT, zclSampleLight_ProcessIncomingMsg);.All
Timer_*APIs have becomeUtilTimer_*.Updated third parameter for
CUI_statusLineResourceRequest,const bool _refreshIndset tofalsein the default application.Any other Z-Stack 3.6.0+ application changes to the Z-Stack 4.3.0 file, if not pertaining to the items listed above, should be added accordingly.
Note
Difference comparison software is recommended for discerning all differences between software stacks.