![]() |
![]() |
TI-15.4 Stack API
4.10.00.12
|
#include <api_mac.h>
Data Fields | |
uint16_t | panID |
uint16_t | shortAddr |
ApiMac_sAddrExt_t | extAddr |
bool | exempt |
uint32_t | frameCounter |
uint8_t | keyIdLookupDataSize |
uint8_t | keyIdLookupData [APIMAC_MAX_KEY_LOOKUP_LEN] |
bool | uniqueDevice |
bool | duplicateDevFlag |
Structure to pass information to the ApiMac_secAddDevice().
uint16_t _apimac_secadddevice::panID |
PAN ID of the new device
uint16_t _apimac_secadddevice::shortAddr |
short address of the new device
ApiMac_sAddrExt_t _apimac_secadddevice::extAddr |
extended address of the new device
bool _apimac_secadddevice::exempt |
Device descriptor exempt field value (true or false), setting this field to true means that this device can override the minimum security level setting.
uint32_t _apimac_secadddevice::frameCounter |
Frame Counter
uint8_t _apimac_secadddevice::keyIdLookupDataSize |
key ID lookup data size as it is stored in PIB, (i.e., 0 for 5 bytes, 1 for 9 bytes).
uint8_t _apimac_secadddevice::keyIdLookupData[APIMAC_MAX_KEY_LOOKUP_LEN] |
key ID lookup data, to look for the key table entry and create proper key device descriptor for this device.
bool _apimac_secadddevice::uniqueDevice |
key device descriptor uniqueDevice field value (true or false)
bool _apimac_secadddevice::duplicateDevFlag |
A flag (true or false) to indicate whether the device entry should be duplicated even for the keys that do not match the key ID lookup data. The device descriptors that are pointed by the key device descriptors that do not match the key ID lookup data shall not update the frame counter based on the frameCounter argument to this function or shall set the frame counter to zero when the entry is newly created.