![]() |
![]() |
TI-15.4 Stack API
4.10.00.12
|
#include <api_mac.h>
Data Fields | |
uint32_t | startTime |
uint16_t | panId |
uint8_t | logicalChannel |
uint8_t | channelPage |
uint8_t | phyID |
uint8_t | beaconOrder |
uint8_t | superframeOrder |
bool | panCoordinator |
bool | batteryLifeExt |
bool | coordRealignment |
ApiMac_sec_t | realignSec |
ApiMac_sec_t | beaconSec |
ApiMac_mpmParams_t | mpmParams |
bool | startFH |
MLME start request type
uint32_t _apimac_mlmestartreq::startTime |
The time to begin transmitting beacons relative to the received beacon
uint16_t _apimac_mlmestartreq::panId |
The PAN ID to use. This parameter is ignored if panCoordinator is FALSE
uint8_t _apimac_mlmestartreq::logicalChannel |
The logical channel to use. This parameter is ignored if panCoordinator is FALSE
uint8_t _apimac_mlmestartreq::channelPage |
The channel page to use. This parameter is ignored if panCoordinator is FALSE
uint8_t _apimac_mlmestartreq::phyID |
PHY ID corresponding to the PHY descriptor to use
uint8_t _apimac_mlmestartreq::beaconOrder |
The exponent used to calculate the beacon interval
uint8_t _apimac_mlmestartreq::superframeOrder |
The exponent used to calculate the superframe duration
bool _apimac_mlmestartreq::panCoordinator |
Set to TRUE to start a network as PAN coordinator
bool _apimac_mlmestartreq::batteryLifeExt |
If this value is TRUE, the receiver is disabled after MAC_BATT_LIFE_EXT_PERIODS full backoff periods following the interframe spacing period of the beacon frame
bool _apimac_mlmestartreq::coordRealignment |
Set to TRUE to transmit a coordinator realignment prior to changing the superframe configuration
ApiMac_sec_t _apimac_mlmestartreq::realignSec |
Security parameters for the coordinator realignment frame
ApiMac_sec_t _apimac_mlmestartreq::beaconSec |
Security parameters for the beacon frame
ApiMac_mpmParams_t _apimac_mlmestartreq::mpmParams |
MPM (multi-PHY layer management) parameters
bool _apimac_mlmestartreq::startFH |
Indicates whether frequency hopping needs to be enabled