Radio Software Bundle (rflib) 5.50.00.31 Release Notes
Table of Contents
Introduction
The Radio Software Bundle (RFLib) component for CC13x2 and CC26x2 consists of products that were previously hosted in different locations and distributed through TIDRIVERS, TIDRIVERS examples and DriverLib:
- The high-level RF driver
- SysConfig meta data for configuring the RF driver and the front-end
- SysConfig meta data for configuring radio PHYs
- Low-level radio access functions used by the RF driver
- RF Core firmware patches for various PHYs
- API documentation
Documentation
The following documentation is included in RFLib.
- RFLib Software Manifest
- API documentation
- Release Notes (this document)
Disclaimer
RF settings and patches for the cc13x2x7_cc26x2x7 and cc13x1_cc26x1 device families are in alpha state. They are not fully characterized and have only been tested in a limited manner. Support for certain settings and PHYs may be removed in the future.
Please consider this content for evaluation purposes only.
What’s New
| ID | Summary |
|---|---|
| RFDRIVER-307 | Add support for loading rftrim values from FCFG1 on cc13x2_c26x1 devices |
| SRFSTUDIO-3010 | SYSCFG: Radioconfig will replace empty (containing only 0xFFFFFFFF terminator) override arrays with NULL |
| SRFSTUDIO-2997 | Release functional settings for cc13x2x7_cc26x2x7 devices |
| SRFSTUDIO-3012 | Release preview radio settings for cc13x2_cc26x1 devices. |
| SRFSTUDIO-2993 | SYSCFG: Rename LAUNCHXL-CC2652RB to LP_CC2652RB in radioconfig |
| SRFSTUDIO-2915 | SYSCFG: Add device support for CC2672R3 |
Fixed Issues
| ID | Summary |
|---|---|
| RFCORE-699 | Fixed issue where protocol ID was incorrect in IQ dump MCE patch |
| RFCORE-696 | Fixed an issue with bit ordering feature for IEEE 802.15.4g did not work with repeated mode |
| SRFSTUDIO-2940 | SYSCFG: Fixed an issue where changing RF Design Front-end for 2.4 GHz option caused build errors |
| SRFSTUDIO-3003 | SYSCFG: Fixed issue where PHY type was not preserved when changing frequency band |
| SRFSTUDIO-2751 | SYSCFG: Fixed an issue where TX power would not be preserved when changing boards |
| SRFSTUDIO-3006 | Mismatch in CMD_BLE5_SCANNER parameter struct |
Known Issues
| ID | Summary |
|---|---|
| None | None |
Upgrade and Compatibility Information
This release breaks compatibility with previous releases of the CC13x2/CC26x2 RF driver in the following ways:
- None known
Versioning
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.