TI BLE5-Stack API Documentation
2.02.01.00
|
Typedefs | |
typedef bStatus_t(* | pfnGATTAuthorizeAttrCB_t) (uint16 connHandle, gattAttribute_t *pAttr, uint8 opcode) |
Callback function prototype to authorize a Read or Write operation on a given attribute. More... | |
typedef bStatus_t(* | pfnGATTReadAttrCB_t) (uint16 connHandle, gattAttribute_t *pAttr, uint8 *pValue, uint16 *pLen, uint16 offset, uint16 maxLen, uint8 method) |
Callback function prototype to read an attribute value. More... | |
typedef bStatus_t(* | pfnGATTWriteAttrCB_t) (uint16 connHandle, gattAttribute_t *pAttr, uint8 *pValue, uint16 len, uint16 offset, uint8 method) |
Callback function prototype to write an attribute value. More... | |
typedef bStatus_t(* pfnGATTAuthorizeAttrCB_t) (uint16 connHandle, gattAttribute_t *pAttr, uint8 opcode) |
Callback function prototype to authorize a Read or Write operation on a given attribute.
connHandle | - connection request was received on |
pAttr | - pointer to attribute |
opcode | - request opcode (ATT_READ_REQ or ATT_WRITE_REQ) |
typedef bStatus_t(* pfnGATTReadAttrCB_t) (uint16 connHandle, gattAttribute_t *pAttr, uint8 *pValue, uint16 *pLen, uint16 offset, uint16 maxLen, uint8 method) |
Callback function prototype to read an attribute value.
connHandle | - connection request was received on |
pAttr | - pointer to attribute |
pValue | - pointer to data to be read (to be returned) |
pLen | - length of data (to be returned) |
offset | - offset of the first octet to be read |
maxLen | - maximum length of data to be read |
method | - type of read message |
typedef bStatus_t(* pfnGATTWriteAttrCB_t) (uint16 connHandle, gattAttribute_t *pAttr, uint8 *pValue, uint16 len, uint16 offset, uint8 method) |
Callback function prototype to write an attribute value.
connHandle | - connection request was received on |
pAttr | - pointer to attribute |
pValue | - pointer to data to be written |
pLen | - length of data |
offset | - offset of the first octet to be written |
method | - type of write message |