Data Fields
TemperatureCC26X2_Config Struct Reference

Temperature driver configuration struct for CC26X2. More...

#include <TemperatureCC26X2.h>

Data Fields

uint8_t intPriority
 Temperature sensor's interrupt priority. More...
 

Detailed Description

Temperature driver configuration struct for CC26X2.

This struct globally controls configuration settings for the CC26X2 Temperature driver.

The CC26X2 Temperature driver implementation links against a structure of this type named TemperatureCC26X2_config.

This structure must be allocated and configured by the application. If SysConfig is used, this struct will be automatically created when the Temperature module is used in SysConfig.

Field Documentation

§ intPriority

uint8_t TemperatureCC26X2_Config::intPriority

Temperature sensor's interrupt priority.

The interrupt line is shared between the temperature sensor and the battery voltage monitor on CC26X2

The CC26X2 uses three of the priority bits, meaning ~0 has the same effect as (7 << 5).

(7 << 5) will apply the lowest priority.

(1 << 5) will apply the highest priority.

Setting the priority to 0 is not supported by this driver.

HWI's with priority 0 ignore the HWI dispatcher to support zero-latency interrupts, thus invalidating the critical sections.


The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale