Functions | Variables
doxygen_drivers.txt File Reference

Functions

This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming interface (API) which enables seamless migration across the SimpleLink SDK portfolio. Unless specifically stated otherwise
 [drivers_common_overview] More...
 
This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating system (RTOS) application. All TI-Driver implementations utilize the Power driver APIs to ensure low power consumption at all times. The drivers support TI-RTOS(SYS/BIOS) and NoRTOS with examples provided for each variant. Lastly
 
This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par and close the driver Unless otherwise the initialization< b > may be called multiple times by the application It is only required that the initialization is done once For drivers which have an open< b > it must be called per instance of the driver to be used Each instance of the driver corresponds to a unique index in the ref< b > Driver_config</b > Multiple software entities may use the same driver concurrently For a Bluetooth or WiFi stack may utilize a driver instance The application may concurrently use the same driver assuming it has opened a unique instance of the driver Let s examine the ADC driver for example include Driver_init h A couple observations from this code ADC_init (). 4. We have to create a handle for our ADC driver instance. This is done by calling ADC_open() with our desired config index. Once a handle has been created the driver instance is ready for use. Each index can only be opened once! 4. In this simple example
 Function to initialize the ADC driver. More...
 
This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par and close the driver Unless otherwise the initialization< b > may be called multiple times by the application It is only required that the initialization is done once For drivers which have an open< b > it must be called per instance of the driver to be used Each instance of the driver corresponds to a unique index in the ref< b > Driver_config</b > Multiple software entities may use the same driver concurrently For a Bluetooth or WiFi stack may utilize a driver instance The application may concurrently use the same driver assuming it has opened a unique instance of the driver Let s examine the ADC driver for example include Driver_init h A couple observations from this code we use the ADC_convert () API. 5. A driver instance can be closed and re-open. For our simple example
 

Variables

This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par Features
 
This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par open
 
This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par use
 
This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par and close the driver Unless otherwise stated
 
This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par and close the driver Unless otherwise the initialization function
 
This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par and close the driver Unless otherwise the initialization< b > Driver_init</b >
 
This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par and close the driver Unless otherwise the initialization< b > may be called multiple times by the application It is only required that the initialization is done once For drivers which have an open< b > Driver_open</b >
 
This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par and close the driver Unless otherwise the initialization< b > may be called multiple times by the application It is only required that the initialization is done once For drivers which have an open< b > it must be called per instance of the driver to be used Each instance of the driver corresponds to a unique index in the ref driver_configuration
 
This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par and close the driver Unless otherwise the initialization< b > may be called multiple times by the application It is only required that the initialization is done once For drivers which have an open< b > it must be called per instance of the driver to be used Each instance of the driver corresponds to a unique index in the ref< b > Driver_config</b > Multiple software entities may use the same driver concurrently For example
 
This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par and close the driver Unless otherwise the initialization< b > may be called multiple times by the application It is only required that the initialization is done once For drivers which have an open< b > it must be called per instance of the driver to be used Each instance of the driver corresponds to a unique index in the ref< b > Driver_config</b > Multiple software entities may use the same driver concurrently For a Bluetooth or WiFi stack may utilize a driver instance The application may concurrently use the same driver assuming it has opened a unique instance of the driver Let s examine the ADC driver for example include Driver_init h A couple observations from this code we use the that s all we need However
 
This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par and close the driver Unless otherwise the initialization< b > may be called multiple times by the application It is only required that the initialization is done once For drivers which have an open< b > it must be called per instance of the driver to be used Each instance of the driver corresponds to a unique index in the ref< b > Driver_config</b > Multiple software entities may use the same driver concurrently For a Bluetooth or WiFi stack may utilize a driver instance The application may concurrently use the same driver assuming it has opened a unique instance of the driver Let s examine the ADC driver for example include Driver_init h A couple observations from this code we use the that s all we need for full details on the ADC and other drivers
 
This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par and close the driver Unless otherwise the initialization< b > may be called multiple times by the application It is only required that the initialization is done once For drivers which have an open< b > it must be called per instance of the driver to be used Each instance of the driver corresponds to a unique index in the ref< b > Driver_config</b > Multiple software entities may use the same driver concurrently For a Bluetooth or WiFi stack may utilize a driver instance The application may concurrently use the same driver assuming it has opened a unique instance of the driver Let s examine the ADC driver for example include Driver_init h A couple observations from this code we use the that s all we need for full details on the ADC and other reference the< b > Drivers and Documentation</b > section below endparblock *******************************************************************************The Display driver is designed abstract to operations &considerations specific to a given output method *******************************************************************************< TABLE >< TR align="center">< TH > Display Driver Interface</TH >< TH > Implementations</TH ></TR >< TR align="center">< TD > ref Display h</TD >< TD > ref DisplayHost h n ref DisplayUart h</TD ></TR ></TABLE > *******************************************************************************< TABLE >< TR align="center">< TH > Display Driver Interface</TH >< TH > Implementations</TH ></TR >< TR align="center">< TD > ref Display h</TD >< TD > ref DisplayDogm1286 h n ref DisplayHost h n ref DisplayExt h n ref DisplayUart h</TD ></TR ></TABLE > *******************************************************************************The NoRTOS framework module is provided to enable use of drivers without an underlying operating system The module provides interfaces used by drivers to perform delays
 [drivers_common_overview] More...
 
This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par and close the driver Unless otherwise the initialization< b > may be called multiple times by the application It is only required that the initialization is done once For drivers which have an open< b > it must be called per instance of the driver to be used Each instance of the driver corresponds to a unique index in the ref< b > Driver_config</b > Multiple software entities may use the same driver concurrently For a Bluetooth or WiFi stack may utilize a driver instance The application may concurrently use the same driver assuming it has opened a unique instance of the driver Let s examine the ADC driver for example include Driver_init h A couple observations from this code we use the that s all we need for full details on the ADC and other reference the< b > Drivers and Documentation</b > section below endparblock *******************************************************************************The Display driver is designed abstract to operations &considerations specific to a given output method *******************************************************************************< TABLE >< TR align="center">< TH > Display Driver Interface</TH >< TH > Implementations</TH ></TR >< TR align="center">< TD > ref Display h</TD >< TD > ref DisplayHost h n ref DisplayUart h</TD ></TR ></TABLE > *******************************************************************************< TABLE >< TR align="center">< TH > Display Driver Interface</TH >< TH > Implementations</TH ></TR >< TR align="center">< TD > ref Display h</TD >< TD > ref DisplayDogm1286 h n ref DisplayHost h n ref DisplayExt h n ref DisplayUart h</TD ></TR ></TABLE > *******************************************************************************The NoRTOS framework module is provided to enable use of drivers without an underlying operating system The module provides interfaces used by drivers to perform block execution
 

Function Documentation

§ interface()

This file contains snippets to be used in the TI Driver s documentation******************************************************************************* TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming interface ( API  )

[drivers_common_overview]

§ system()

This file contains snippets to be used in the TI Driver s documentation******************************************************************************* TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating system ( RTOS  )

§ ADC_init()

This file contains snippets to be used in the TI Driver s documentation******************************************************************************* TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par and close the driver Unless otherwise the initialization<b> may be called multiple times by the application It is only required that the initialization is done once For drivers which have an open<b> it must be called per instance of the driver to be used Each instance of the driver corresponds to a unique index in the ref<b> Driver_config</b> Multiple software entities may use the same driver concurrently For a Bluetooth or WiFi stack may utilize a driver instance The application may concurrently use the same driver assuming it has opened a unique instance of the driver Let s examine the ADC driver for example include Driver_init h A couple observations from this code ADC_init ( void  )

Function to initialize the ADC driver.

This function must also be called before any other ADC driver APIs.

§ ADC_convert()

This file contains snippets to be used in the TI Driver s documentation******************************************************************************* TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par and close the driver Unless otherwise the initialization<b> may be called multiple times by the application It is only required that the initialization is done once For drivers which have an open<b> it must be called per instance of the driver to be used Each instance of the driver corresponds to a unique index in the ref<b> Driver_config</b> Multiple software entities may use the same driver concurrently For a Bluetooth or WiFi stack may utilize a driver instance The application may concurrently use the same driver assuming it has opened a unique instance of the driver Let s examine the ADC driver for example include Driver_init h A couple observations from this code we use the ADC_convert ( )

Variable Documentation

§ Features

This file contains snippets to be used in the TI Driver s documentation******************************************************************************* TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par Features

§ open

This file contains snippets to be used in the TI Driver s documentation******************************************************************************* TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par open

§ use

This file contains snippets to be used in the TI Driver s documentation******************************************************************************* TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par use

§ stated

This file contains snippets to be used in the TI Driver s documentation******************************************************************************* TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par and close the driver Unless otherwise stated

§ function

This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par and close the driver Unless otherwise the initialization< b > may be called multiple times by the application It is only required that the initialization is done once For drivers which have an open function

§ Driver_init

This file contains snippets to be used in the TI Driver s documentation******************************************************************************* TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par and close the driver Unless otherwise the initialization<b> Driver_init</b >

§ Driver_open

This file contains snippets to be used in the TI Driver s documentation******************************************************************************* TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par and close the driver Unless otherwise the initialization<b> may be called multiple times by the application It is only required that the initialization is done once For drivers which have an open<b> Driver_open</b >

§ driver_configuration

This file contains snippets to be used in the TI Driver s documentation******************************************************************************* TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par and close the driver Unless otherwise the initialization<b> may be called multiple times by the application It is only required that the initialization is done once For drivers which have an open<b> it must be called per instance of the driver to be used Each instance of the driver corresponds to a unique index in the ref driver_configuration

§ example

This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par and close the driver Unless otherwise the initialization< b > may be called multiple times by the application It is only required that the initialization is done once For drivers which have an open< b > it must be called per instance of the driver to be used Each instance of the driver corresponds to a unique index in the ref< b > Driver_config</b > Multiple software entities may use the same driver concurrently For a Bluetooth or WiFi stack may utilize a driver instance The application may concurrently use the same driver assuming it has opened a unique instance of the driver Let s examine the ADC driver for example include Driver_init h A couple observations from this code example

§ However

This file contains snippets to be used in the TI Driver s documentation******************************************************************************* TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par and close the driver Unless otherwise the initialization<b> may be called multiple times by the application It is only required that the initialization is done once For drivers which have an open<b> it must be called per instance of the driver to be used Each instance of the driver corresponds to a unique index in the ref<b> Driver_config</b> Multiple software entities may use the same driver concurrently For a Bluetooth or WiFi stack may utilize a driver instance The application may concurrently use the same driver assuming it has opened a unique instance of the driver Let s examine the ADC driver for example include Driver_init h A couple observations from this code we use the that s all we need However

§ drivers

This file contains snippets to be used in the TI Driver s documentation******************************************************************************* TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par and close the driver Unless otherwise the initialization<b> may be called multiple times by the application It is only required that the initialization is done once For drivers which have an open<b> it must be called per instance of the driver to be used Each instance of the driver corresponds to a unique index in the ref<b> Driver_config</b> Multiple software entities may use the same driver concurrently For a Bluetooth or WiFi stack may utilize a driver instance The application may concurrently use the same driver assuming it has opened a unique instance of the driver Let s examine the ADC driver for example include Driver_init h A couple observations from this code we use the that s all we need for full details on the ADC and other drivers

§ delays

This file contains snippets to be used in the TI Driver s documentation******************************************************************************* TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par and close the driver Unless otherwise the initialization<b> may be called multiple times by the application It is only required that the initialization is done once For drivers which have an open<b> it must be called per instance of the driver to be used Each instance of the driver corresponds to a unique index in the ref<b> Driver_config</b> Multiple software entities may use the same driver concurrently For a Bluetooth or WiFi stack may utilize a driver instance The application may concurrently use the same driver assuming it has opened a unique instance of the driver Let s examine the ADC driver for example include Driver_init h A couple observations from this code we use the that s all we need for full details on the ADC and other reference the<b> Drivers and Documentation</b> section below endparblock******************************************************************************* The Display driver is designed abstract to operations& considerations specific to a given output method*******************************************************************************<TABLE><TR align ="center"><TH> Display Driver Interface</TH><TH> Implementations</TH></TR><TR align ="center"><TD> ref Display h</TD><TD> ref DisplayHost h n ref DisplayUart h</TD></TR></TABLE> *******************************************************************************<TABLE><TR align ="center"><TH> Display Driver Interface</TH><TH> Implementations</TH></TR><TR align ="center"><TD> ref Display h</TD><TD> ref DisplayDogm1286 h n ref DisplayHost h n ref DisplayExt h n ref DisplayUart h</TD></TR></TABLE> ******************************************************************************* The NoRTOS framework module is provided to enable use of drivers without an underlying operating system The module provides interfaces used by drivers to perform delays

[drivers_common_overview]

[drivers_common_display] [drivers_common_display] [drivers_common_display_table] [drivers_common_display_table] [drivers_full_display_table] [drivers_full_display_table] [drivers_common_nortos]

§ execution

This file contains snippets to be used in the TI Driver s documentation******************************************************************************* TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par and close the driver Unless otherwise the initialization<b> may be called multiple times by the application It is only required that the initialization is done once For drivers which have an open<b> it must be called per instance of the driver to be used Each instance of the driver corresponds to a unique index in the ref<b> Driver_config</b> Multiple software entities may use the same driver concurrently For a Bluetooth or WiFi stack may utilize a driver instance The application may concurrently use the same driver assuming it has opened a unique instance of the driver Let s examine the ADC driver for example include Driver_init h A couple observations from this code we use the that s all we need for full details on the ADC and other reference the<b> Drivers and Documentation</b> section below endparblock******************************************************************************* The Display driver is designed abstract to operations& considerations specific to a given output method*******************************************************************************<TABLE><TR align ="center"><TH> Display Driver Interface</TH><TH> Implementations</TH></TR><TR align ="center"><TD> ref Display h</TD><TD> ref DisplayHost h n ref DisplayUart h</TD></TR></TABLE> *******************************************************************************<TABLE><TR align ="center"><TH> Display Driver Interface</TH><TH> Implementations</TH></TR><TR align ="center"><TD> ref Display h</TD><TD> ref DisplayDogm1286 h n ref DisplayHost h n ref DisplayExt h n ref DisplayUart h</TD></TR></TABLE> ******************************************************************************* The NoRTOS framework module is provided to enable use of drivers without an underlying operating system The module provides interfaces used by drivers to perform block execution
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale