TI-15.4 Stack API
3.40.00.09
|
#include <api_mac.h>
Data Fields | |
uint8_t | key [APIMAC_KEY_MAX_LEN] |
uint32_t | frameCounter |
uint16_t | replaceKeyIndex |
bool | newKeyFlag |
uint8_t | lookupDataSize |
uint8_t | lookupData [APIMAC_MAX_KEY_LOOKUP_LEN] |
Structure to pass information to the ApiMac_secAddKeyInitFrameCounter().
uint8_t _apimac_secaddkeyinitframecounter::key[APIMAC_KEY_MAX_LEN] |
Key
uint32_t _apimac_secaddkeyinitframecounter::frameCounter |
Frame Counter
uint16_t _apimac_secaddkeyinitframecounter::replaceKeyIndex |
Key index of the mac security key table where the key needs to be written
bool _apimac_secaddkeyinitframecounter::newKeyFlag |
If set to true, the function will duplicate the device table enteries associated with the previous key, and associate it with the key. If set to false, the function will not alter device table entries associated with whatever key that was stored in the key table location as designated by replaceKeyIndex.
uint8_t _apimac_secaddkeyinitframecounter::lookupDataSize |
Key ID lookup data size as it is stored in PIB, i.e., 0 for 5 bytes, 1 for 9 bytes.
uint8_t _apimac_secaddkeyinitframecounter::lookupData[APIMAC_MAX_KEY_LOOKUP_LEN] |
Key ID lookup data, to look for the key table entry and create proper key device descriptor for this device.