TI-15.4 Stack API
3.40.00.09
|
#include <api_mac.h>
Data Fields | |
uint8_t | beaconOrder |
uint8_t | superFrameOrder |
uint8_t | finalCapSlot |
uint8_t | eBeaconOrder |
uint8_t | offsetTimeSlot |
uint8_t | capBackOff |
uint16_t | eBeaconOrderNBPAN |
Coexistence Information element content type
uint8_t _apimac_coexist::beaconOrder |
Beacon Order field shall specify the transmission interval of the beacon
uint8_t _apimac_coexist::superFrameOrder |
Superframe Order field shall specify the length of time during which the superframe is active (i.e., receiver enabled), including the Beacon frametransmission time
uint8_t _apimac_coexist::finalCapSlot |
Final CAP slot
uint8_t _apimac_coexist::eBeaconOrder |
Enhanced Beacon Order field specifies the transmission interval of the Enhanced Beacon frames in a beacon enabled network
uint8_t _apimac_coexist::offsetTimeSlot |
Time offset between periodic beacon and the Enhanced Beacon.
uint8_t _apimac_coexist::capBackOff |
Actual slot position in which the Enhanced Beacon frame is transmitted due to the backoff procedure in the CAP
uint16_t _apimac_coexist::eBeaconOrderNBPAN |
NBPAN Enhanced Beacon Order field specifies the transmission interval between consecutive Enhanced Beacon frames in the nonbeacon-enabled mode