#include <rf_ble_cmd.h>
|
struct { |
uint8_t channel:6 |
| The channel on which the packet was received, provided channel is in the range 0–39; otherwise 0x3F. More...
|
|
uint8_t bIgnore:1 |
| 1 if the packet is marked as ignored, 0 otherwise More...
|
|
uint8_t bCrcErr:1 |
| 1 if the packet was received with CRC error, 0 otherwise More...
|
|
} | status |
|
§ channel
uint8_t rfc_bleRxStatus_s::channel |
The channel on which the packet was received, provided channel is in the range 0–39; otherwise 0x3F.
§ bIgnore
uint8_t rfc_bleRxStatus_s::bIgnore |
1 if the packet is marked as ignored, 0 otherwise
§ bCrcErr
uint8_t rfc_bleRxStatus_s::bCrcErr |
1 if the packet was received with CRC error, 0 otherwise
§ status
struct { ... } rfc_bleRxStatus_s::status |
The documentation for this struct was generated from the following file: