![]() |
![]() |
rflib
|
Proprietary Mode Advanced Receive Command. More...
#include <rf_prop_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number 0x3804. More... | |
uint16_t | status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More... | |
rfc_radioOp_t * | pNextOp |
Pointer to the next operation to run after this operation is done. More... | |
ratmr_t | startTime |
Absolute or relative start time (depending on the value of startTrigger ) More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | startTrigger |
Identification of the trigger that starts the operation. More... | |
struct { | |
uint8_t rule:4 | |
Condition for running next command: Rule for how to proceed. More... | |
uint8_t nSkip:4 | |
Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More... | |
} | condition |
struct { | |
uint8_t bFsOff:1 | |
0: Keep frequency synth on after command 1: Turn frequency synth off after command More... | |
uint8_t bRepeatOk:1 | |
0: End operation after receiving a packet correctly 1: Go back to sync search after receiving a packet correctly More... | |
uint8_t bRepeatNok:1 | |
0: End operation after receiving a packet with CRC error 1: Go back to sync search after receiving a packet with CRC error More... | |
uint8_t bUseCrc:1 | |
0: Do not check CRC 1: Check CRC More... | |
uint8_t bCrcIncSw:1 | |
0: Do not include sync word in CRC calculation 1: Include sync word in CRC calculation More... | |
uint8_t bCrcIncHdr:1 | |
0: Do not include header in CRC calculation 1: Include header in CRC calculation More... | |
uint8_t endType:1 | |
0: Packet is received to the end if end trigger happens after sync is obtained 1: Packet reception is stopped if end trigger happens More... | |
uint8_t filterOp:1 | |
0: Stop receiver and restart sync search on address mismatch 1: Receive packet and mark it as ignored on address mismatch More... | |
} | pktConf |
struct { | |
uint8_t bAutoFlushIgnored:1 | |
If 1, automatically discard ignored packets from RX queue. More... | |
uint8_t bAutoFlushCrcErr:1 | |
If 1, automatically discard packets with CRC error from RX queue. More... | |
uint8_t __pad0__:1 | |
uint8_t bIncludeHdr:1 | |
If 1, include the received header or length byte in the stored packet; otherwise discard it. More... | |
uint8_t bIncludeCrc:1 | |
If 1, include the received CRC field in the stored packet; otherwise discard it. More... | |
uint8_t bAppendRssi:1 | |
If 1, append an RSSI byte to the packet in the RX queue. More... | |
uint8_t bAppendTimestamp:1 | |
If 1, append a timestamp to the packet in the RX queue. More... | |
uint8_t bAppendStatus:1 | |
If 1, append a status byte to the packet in the RX queue. More... | |
} | rxConf |
RX configuration. More... | |
uint32_t | syncWord0 |
Sync word to listen for. More... | |
uint32_t | syncWord1 |
Alternative sync word if non-zero. More... | |
uint16_t | maxPktLen |
Packet length for fixed length, maximum packet length for variable length 0: Unlimited or unknown length. More... | |
struct { | |
uint16_t numHdrBits:6 | |
Number of bits in header (0–32) More... | |
uint16_t lenPos:5 | |
Position of length field in header (0–31) More... | |
uint16_t numLenBits:5 | |
Number of bits in length field (0–16) More... | |
} | hdrConf |
struct { | |
uint16_t addrType:1 | |
0: Address after header 1: Address in header More... | |
uint16_t addrSize:5 | |
If addrType = 0: Address size in bytesIf addrType = 1: Address size in bits. More... | |
uint16_t addrPos:5 | |
If addrType = 1: Bit position of address in headerIf addrType = 0: Non-zero to extend address with sync word identifier. More... | |
uint16_t numAddr:5 | |
Number of addresses in address list. More... | |
} | addrConf |
int8_t | lenOffset |
Signed value to add to length field. More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | endTrigger |
Trigger classifier for ending the operation. More... | |
ratmr_t | endTime |
Time used together with endTrigger for ending the operation. More... | |
uint8_t * | pAddr |
Pointer to address list. More... | |
dataQueue_t * | pQueue |
Pointer to receive queue. More... | |
uint8_t * | pOutput |
Pointer to output structure. More... | |
Proprietary Mode Advanced Receive Command.
uint16_t rfc_CMD_PROP_RX_ADV_s::commandNo |
The command ID number 0x3804.
uint16_t rfc_CMD_PROP_RX_ADV_s::status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.
rfc_radioOp_t* rfc_CMD_PROP_RX_ADV_s::pNextOp |
Pointer to the next operation to run after this operation is done.
ratmr_t rfc_CMD_PROP_RX_ADV_s::startTime |
Absolute or relative start time (depending on the value of startTrigger
)
uint8_t rfc_CMD_PROP_RX_ADV_s::triggerType |
The type of trigger.
uint8_t rfc_CMD_PROP_RX_ADV_s::bEnaCmd |
0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger
uint8_t rfc_CMD_PROP_RX_ADV_s::triggerNo |
The trigger number of the CMD_TRIGGER command that triggers this action.
uint8_t rfc_CMD_PROP_RX_ADV_s::pastTrig |
0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible
struct { ... } rfc_CMD_PROP_RX_ADV_s::startTrigger |
Identification of the trigger that starts the operation.
uint8_t rfc_CMD_PROP_RX_ADV_s::rule |
Condition for running next command: Rule for how to proceed.
uint8_t rfc_CMD_PROP_RX_ADV_s::nSkip |
Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...
struct { ... } rfc_CMD_PROP_RX_ADV_s::condition |
uint8_t rfc_CMD_PROP_RX_ADV_s::bFsOff |
0: Keep frequency synth on after command
1: Turn frequency synth off after command
uint8_t rfc_CMD_PROP_RX_ADV_s::bRepeatOk |
0: End operation after receiving a packet correctly
1: Go back to sync search after receiving a packet correctly
uint8_t rfc_CMD_PROP_RX_ADV_s::bRepeatNok |
0: End operation after receiving a packet with CRC error
1: Go back to sync search after receiving a packet with CRC error
uint8_t rfc_CMD_PROP_RX_ADV_s::bUseCrc |
0: Do not check CRC
1: Check CRC
uint8_t rfc_CMD_PROP_RX_ADV_s::bCrcIncSw |
0: Do not include sync word in CRC calculation
1: Include sync word in CRC calculation
uint8_t rfc_CMD_PROP_RX_ADV_s::bCrcIncHdr |
0: Do not include header in CRC calculation
1: Include header in CRC calculation
uint8_t rfc_CMD_PROP_RX_ADV_s::endType |
0: Packet is received to the end if end trigger happens after sync is obtained
1: Packet reception is stopped if end trigger happens
uint8_t rfc_CMD_PROP_RX_ADV_s::filterOp |
0: Stop receiver and restart sync search on address mismatch
1: Receive packet and mark it as ignored on address mismatch
struct { ... } rfc_CMD_PROP_RX_ADV_s::pktConf |
uint8_t rfc_CMD_PROP_RX_ADV_s::bAutoFlushIgnored |
If 1, automatically discard ignored packets from RX queue.
uint8_t rfc_CMD_PROP_RX_ADV_s::bAutoFlushCrcErr |
If 1, automatically discard packets with CRC error from RX queue.
uint8_t rfc_CMD_PROP_RX_ADV_s::__pad0__ |
uint8_t rfc_CMD_PROP_RX_ADV_s::bIncludeHdr |
If 1, include the received header or length byte in the stored packet; otherwise discard it.
uint8_t rfc_CMD_PROP_RX_ADV_s::bIncludeCrc |
If 1, include the received CRC field in the stored packet; otherwise discard it.
uint8_t rfc_CMD_PROP_RX_ADV_s::bAppendRssi |
If 1, append an RSSI byte to the packet in the RX queue.
uint8_t rfc_CMD_PROP_RX_ADV_s::bAppendTimestamp |
If 1, append a timestamp to the packet in the RX queue.
uint8_t rfc_CMD_PROP_RX_ADV_s::bAppendStatus |
If 1, append a status byte to the packet in the RX queue.
struct { ... } rfc_CMD_PROP_RX_ADV_s::rxConf |
RX configuration.
uint32_t rfc_CMD_PROP_RX_ADV_s::syncWord0 |
Sync word to listen for.
uint32_t rfc_CMD_PROP_RX_ADV_s::syncWord1 |
Alternative sync word if non-zero.
uint16_t rfc_CMD_PROP_RX_ADV_s::maxPktLen |
Packet length for fixed length, maximum packet length for variable length
0: Unlimited or unknown length.
uint16_t rfc_CMD_PROP_RX_ADV_s::numHdrBits |
Number of bits in header (0–32)
uint16_t rfc_CMD_PROP_RX_ADV_s::lenPos |
Position of length field in header (0–31)
uint16_t rfc_CMD_PROP_RX_ADV_s::numLenBits |
Number of bits in length field (0–16)
struct { ... } rfc_CMD_PROP_RX_ADV_s::hdrConf |
uint16_t rfc_CMD_PROP_RX_ADV_s::addrType |
0: Address after header
1: Address in header
uint16_t rfc_CMD_PROP_RX_ADV_s::addrSize |
If addrType
= 0: Address size in bytes
If addrType
= 1: Address size in bits.
uint16_t rfc_CMD_PROP_RX_ADV_s::addrPos |
If addrType
= 1: Bit position of address in header
If addrType
= 0: Non-zero to extend address with sync word identifier.
uint16_t rfc_CMD_PROP_RX_ADV_s::numAddr |
Number of addresses in address list.
struct { ... } rfc_CMD_PROP_RX_ADV_s::addrConf |
int8_t rfc_CMD_PROP_RX_ADV_s::lenOffset |
Signed value to add to length field.
struct { ... } rfc_CMD_PROP_RX_ADV_s::endTrigger |
Trigger classifier for ending the operation.
ratmr_t rfc_CMD_PROP_RX_ADV_s::endTime |
Time used together with endTrigger
for ending the operation.
uint8_t* rfc_CMD_PROP_RX_ADV_s::pAddr |
Pointer to address list.
dataQueue_t* rfc_CMD_PROP_RX_ADV_s::pQueue |
Pointer to receive queue.
uint8_t* rfc_CMD_PROP_RX_ADV_s::pOutput |
Pointer to output structure.