![]() |
![]() |
rflib
|
HID Transmit Command with Auto Retransmission. More...
#include <rf_hid_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number 0x5801. More... | |
uint16_t | status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More... | |
rfc_radioOp_t * | pNextOp |
Pointer to the next operation to run after this operation is done. More... | |
ratmr_t | startTime |
Absolute or relative start time (depending on the value of startTrigger ) More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | startTrigger |
Identification of the trigger that starts the operation. More... | |
struct { | |
uint8_t rule:4 | |
Condition for running next command: Rule for how to proceed. More... | |
uint8_t nSkip:4 | |
Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More... | |
} | condition |
struct { | |
uint8_t bFsOff:1 | |
0: Keep frequency synth on after command 1: Turn frequency synth off after command More... | |
uint8_t bAutoRetransmit:1 | |
0: Do not listen for ACK 1: Listen for ACK and retransmit if missing More... | |
uint8_t bVarLen:1 | |
0: Fixed length mode 1: Variable length mode More... | |
uint8_t hdrMode:1 | |
0: 9-bit header 1: 10-bit header More... | |
uint8_t bIncludeAddr:1 | |
0: Do not include address byte after sync word 1: Include address byte after sync word More... | |
uint8_t hdrConf:2 | |
0: Automatically generate header (no header byte in buffer) 1: Insert NO_ACK field from TX buffer 2: Insert SEQ field from TX buffer 3: Insert SEQ and NO_ACK field from TX buffer More... | |
uint8_t bFixedTxLen:1 | |
0: Use actual length in header when sending packet 1: Use fixed word in length field of header when sending packet (only for peer without variable length packets) More... | |
} | pktConf |
struct { | |
uint8_t bAutoFlushIgnored:1 | |
If 1, automatically remove ignored packets (RX) or empty ACKs (TX) from RX queue. More... | |
uint8_t bAutoFlushCrcErr:1 | |
If 1, automatically remove packets with CRC error from Rx queue. More... | |
uint8_t bIncludeAddr:1 | |
If 1, the received address byte is included in the Rx queue. More... | |
uint8_t bIncludeHdr:1 | |
If 1, the received header is included in the Rx queue. More... | |
uint8_t bIncludeCrc:1 | |
If 1, include the received CRC field in the stored packet; otherwise discard it. More... | |
uint8_t bAppendRssi:1 | |
If 1, append an RSSI byte to the packet in the Rx queue. More... | |
uint8_t bAppendStatus:1 | |
If 1, append a status byte to the packet in the Rx queue. More... | |
uint8_t bAppendTimestamp:1 | |
If 1, append a timestamp to the packet in the Rx queue. More... | |
} | rxConf |
Receive entry configuration. More... | |
uint32_t | syncWord |
Sync word to send. More... | |
uint8_t | address |
Address byte. More... | |
uint8_t | seqNo |
Sequence number to use for next packet. More... | |
uint8_t | maxAckLen |
Maximum length of ACKs. More... | |
uint8_t | pktLen |
Length of transmitted packet. More... | |
uint8_t | maxRetrans |
Maximum number of retransmissions. More... | |
struct { | |
uint8_t noAckVal:2 | |
0: Set automatic NO_ACK value to inverse of bAutoRetransmit 1: Set automatic NO_ACK value to bAutoRetransmit 2: Set automatic NO_ACK value to 0 3: Set automatic NO_ACK value to 1 More... | |
uint8_t bAlwaysAutoRetransmit:1 | |
0: Disable auto retransmit if transmitted NO_ACK was 1 1: Never disable auto retransmit More... | |
} | noAckMode |
uint16_t | retransDelay |
Number of RAT ticks from start of transmission of a packet to retransmission. More... | |
uint8_t * | pPkt |
Pointer to transmit queue for packets. More... | |
dataQueue_t * | pRxQueue |
Pointer to receive queue for ACKs. More... | |
rfc_hidRxTxOutput_t * | pOutput |
Pointer to output structure. More... | |
HID Transmit Command with Auto Retransmission.
uint16_t rfc_CMD_HID_TX_s::commandNo |
The command ID number 0x5801.
uint16_t rfc_CMD_HID_TX_s::status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.
rfc_radioOp_t* rfc_CMD_HID_TX_s::pNextOp |
Pointer to the next operation to run after this operation is done.
ratmr_t rfc_CMD_HID_TX_s::startTime |
Absolute or relative start time (depending on the value of startTrigger
)
uint8_t rfc_CMD_HID_TX_s::triggerType |
The type of trigger.
uint8_t rfc_CMD_HID_TX_s::bEnaCmd |
0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger
uint8_t rfc_CMD_HID_TX_s::triggerNo |
The trigger number of the CMD_TRIGGER command that triggers this action.
uint8_t rfc_CMD_HID_TX_s::pastTrig |
0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible
struct { ... } rfc_CMD_HID_TX_s::startTrigger |
Identification of the trigger that starts the operation.
uint8_t rfc_CMD_HID_TX_s::rule |
Condition for running next command: Rule for how to proceed.
uint8_t rfc_CMD_HID_TX_s::nSkip |
Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...
struct { ... } rfc_CMD_HID_TX_s::condition |
uint8_t rfc_CMD_HID_TX_s::bFsOff |
0: Keep frequency synth on after command
1: Turn frequency synth off after command
uint8_t rfc_CMD_HID_TX_s::bAutoRetransmit |
0: Do not listen for ACK
1: Listen for ACK and retransmit if missing
uint8_t rfc_CMD_HID_TX_s::bVarLen |
0: Fixed length mode
1: Variable length mode
uint8_t rfc_CMD_HID_TX_s::hdrMode |
0: 9-bit header
1: 10-bit header
uint8_t rfc_CMD_HID_TX_s::bIncludeAddr |
0: Do not include address byte after sync word
1: Include address byte after sync word
If 1, the received address byte is included in the Rx queue.
uint8_t rfc_CMD_HID_TX_s::hdrConf |
0: Automatically generate header (no header byte in buffer)
1: Insert NO_ACK field from TX buffer
2: Insert SEQ field from TX buffer
3: Insert SEQ and NO_ACK field from TX buffer
uint8_t rfc_CMD_HID_TX_s::bFixedTxLen |
0: Use actual length in header when sending packet
1: Use fixed word in length field of header when sending packet (only for peer without variable length packets)
struct { ... } rfc_CMD_HID_TX_s::pktConf |
uint8_t rfc_CMD_HID_TX_s::bAutoFlushIgnored |
If 1, automatically remove ignored packets (RX) or empty ACKs (TX) from RX queue.
uint8_t rfc_CMD_HID_TX_s::bAutoFlushCrcErr |
If 1, automatically remove packets with CRC error from Rx queue.
uint8_t rfc_CMD_HID_TX_s::bIncludeHdr |
If 1, the received header is included in the Rx queue.
uint8_t rfc_CMD_HID_TX_s::bIncludeCrc |
If 1, include the received CRC field in the stored packet; otherwise discard it.
uint8_t rfc_CMD_HID_TX_s::bAppendRssi |
If 1, append an RSSI byte to the packet in the Rx queue.
uint8_t rfc_CMD_HID_TX_s::bAppendStatus |
If 1, append a status byte to the packet in the Rx queue.
uint8_t rfc_CMD_HID_TX_s::bAppendTimestamp |
If 1, append a timestamp to the packet in the Rx queue.
struct { ... } rfc_CMD_HID_TX_s::rxConf |
Receive entry configuration.
uint32_t rfc_CMD_HID_TX_s::syncWord |
Sync word to send.
uint8_t rfc_CMD_HID_TX_s::address |
Address byte.
uint8_t rfc_CMD_HID_TX_s::seqNo |
Sequence number to use for next packet.
uint8_t rfc_CMD_HID_TX_s::maxAckLen |
Maximum length of ACKs.
uint8_t rfc_CMD_HID_TX_s::pktLen |
Length of transmitted packet.
uint8_t rfc_CMD_HID_TX_s::maxRetrans |
Maximum number of retransmissions.
uint8_t rfc_CMD_HID_TX_s::noAckVal |
0: Set automatic NO_ACK value to inverse of bAutoRetransmit
1: Set automatic NO_ACK value to bAutoRetransmit
2: Set automatic NO_ACK value to 0
3: Set automatic NO_ACK value to 1
uint8_t rfc_CMD_HID_TX_s::bAlwaysAutoRetransmit |
0: Disable auto retransmit if transmitted NO_ACK was 1
1: Never disable auto retransmit
struct { ... } rfc_CMD_HID_TX_s::noAckMode |
uint16_t rfc_CMD_HID_TX_s::retransDelay |
Number of RAT ticks from start of transmission of a packet to retransmission.
uint8_t* rfc_CMD_HID_TX_s::pPkt |
Pointer to transmit queue for packets.
dataQueue_t* rfc_CMD_HID_TX_s::pRxQueue |
Pointer to receive queue for ACKs.
rfc_hidRxTxOutput_t* rfc_CMD_HID_TX_s::pOutput |
Pointer to output structure.