![]() |
![]() |
rflib
|
BLE Update Advertising Payload Command. More...
#include <rf_ble_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number 0x1001. More... | |
uint8_t | payloadType |
0: Advertising data 1: Scan response data More... | |
uint8_t | newLen |
Length of the new payload. More... | |
uint8_t * | pNewData |
Pointer to the buffer containing the new data. More... | |
rfc_bleAdvPar_t * | pParams |
Pointer to the parameter structure to update. More... | |
BLE Update Advertising Payload Command.
uint16_t rfc_CMD_BLE_ADV_PAYLOAD_s::commandNo |
The command ID number 0x1001.
uint8_t rfc_CMD_BLE_ADV_PAYLOAD_s::payloadType |
0: Advertising data
1: Scan response data
uint8_t rfc_CMD_BLE_ADV_PAYLOAD_s::newLen |
Length of the new payload.
uint8_t* rfc_CMD_BLE_ADV_PAYLOAD_s::pNewData |
Pointer to the buffer containing the new data.
rfc_bleAdvPar_t* rfc_CMD_BLE_ADV_PAYLOAD_s::pParams |
Pointer to the parameter structure to update.