|
struct { |
uint8_t bCoExEnable:1 |
| 0: CoEx disabled 1: CoEx enabled More...
|
|
uint8_t bUseREQUEST:1 |
| 0: REQUEST signal inactive 1: REQUEST signal active More...
|
|
uint8_t bUseGRANT:1 |
| 0: GRANT signal inactive 1: GRANT signal active More...
|
|
uint8_t bUsePRIORITY:1 |
| 0: PRIORITY signal inactive 1: PRIORITY signal active More...
|
|
uint8_t bRequestForChain:1 |
| 0: Deassert REQUEST after each RF command 1: Keep REQUEST asserted for entire command chain More...
|
|
} | coExEnable |
|
uint8_t | coExTxRxIndication |
| 0 = RX indication is 0, TX indication is 0 1 = RX indication is 0, TX indication is 1 2 = RX indication is 1, TX indication is 0 3 = RX indication is 1, RX indication is 1 More...
|
|
uint16_t | priorityIndicationTime |
| Time (in us) that the PRIORITY signal will indicate the priority. More...
|
|
struct { |
uint8_t bRequestAsserted:1 |
| READ ONLY. 0 = REQUEST not asserted, 1 = REQUEST is asserted. Will indicate if REQUEST would have been asserted, except if signal is not used. More...
|
|
uint8_t bIgnoreGrantInRxAsserted:1 |
| READ ONLY. 0 = GRANT is checked in RX, 1 = GRANT is not checked in RX. More...
|
|
} | rfCoreCoExStatus |
|
struct { |
uint8_t bUseOverridePriority:1 |
| Bit to override default priority 0: Use default priority 1: use overridePriority priority for entire chain. More...
|
|
uint8_t overridePriority:1 |
| Priority to use if priority is overridden 0: Low priority if bUseOverridePriority = 1 1: High priority if bUseOverridePriority = 1. More...
|
|
uint8_t bUseOverrideRequestForRx:1 |
| Bit to override default request for RX. More...
|
|
uint8_t overrideRequestForRx:1 |
| REQUEST signal override if bUseOverrideRequestForRx = 1, used for entire chain 0: Don't request for RX if bUseOverrideRequestForRx = 1 1: Request for RX if bUseOverrideRequestForRx = 1. More...
|
|
} | overrideConfig |
|
struct { |
uint8_t defaultPriority:1 |
| 0: Default low priority 1: Default high priority More...
|
|
uint8_t bAssertRequestForRx:1 |
| Default "request for RX" behaviour 0: Assert REQUEST for TX operations only 1: Assert REQUEST for both RX and TX operations. More...
|
|
uint8_t bIgnoreGrantInRx:1 |
| 0: Check GRANT in RX and TX 1: Ignore GRANT in RX, check GRANT in TX. Independent of asserting REQUEST for RX. More...
|
|
uint8_t bKeepRequestIfNoGrant:1 |
| 0: Deassert REQUEST if GRANT was not given 1: Keep REQUEST asserted if no GRANT was given More...
|
|
} | cmdBleMasterSlaveConfig |
|
struct { |
uint8_t defaultPriority:1 |
| 0: Default low priority 1: Default high priority More...
|
|
uint8_t bAssertRequestForRx:1 |
| Default "request for RX" behaviour 0: Assert REQUEST for TX operations only 1: Assert REQUEST for both RX and TX operations. More...
|
|
uint8_t bIgnoreGrantInRx:1 |
| 0: Check GRANT in RX and TX 1: Ignore GRANT in RX, check GRANT in TX. Independent of asserting REQUEST for RX. More...
|
|
uint8_t bKeepRequestIfNoGrant:1 |
| 0: Deassert REQUEST if GRANT was not given 1: Keep REQUEST asserted if no GRANT was given More...
|
|
} | cmdBleAdvConfig |
|
struct { |
uint8_t defaultPriority:1 |
| 0: Default low priority 1: Default high priority More...
|
|
uint8_t bAssertRequestForRx:1 |
| Default "request for RX" behaviour 0: Assert REQUEST for TX operations only 1: Assert REQUEST for both RX and TX operations. More...
|
|
uint8_t bIgnoreGrantInRx:1 |
| 0: Check GRANT in RX and TX 1: Ignore GRANT in RX, check GRANT in TX. Independent of asserting REQUEST for RX. More...
|
|
uint8_t bKeepRequestIfNoGrant:1 |
| 0: Deassert REQUEST if GRANT was not given 1: Keep REQUEST asserted if no GRANT was given More...
|
|
} | cmdBleScanConfig |
|
struct { |
uint8_t defaultPriority:1 |
| 0: Default low priority 1: Default high priority More...
|
|
uint8_t bAssertRequestForRx:1 |
| Default "request for RX" behaviour 0: Assert REQUEST for TX operations only 1: Assert REQUEST for both RX and TX operations. More...
|
|
uint8_t bIgnoreGrantInRx:1 |
| 0: Check GRANT in RX and TX 1: Ignore GRANT in RX, check GRANT in TX. Independent of asserting REQUEST for RX. More...
|
|
uint8_t bKeepRequestIfNoGrant:1 |
| 0: Deassert REQUEST if GRANT was not given 1: Keep REQUEST asserted if no GRANT was given More...
|
|
} | cmdBleInitConfig |
|
struct { |
uint8_t defaultPriority:1 |
| 0: Default low priority 1: Default high priority More...
|
|
uint8_t bAssertRequestForRx:1 |
| Default "request for RX" behaviour 0: Assert REQUEST for TX operations only 1: Assert REQUEST for both RX and TX operations. More...
|
|
uint8_t bIgnoreGrantInRx:1 |
| 0: Check GRANT in RX and TX 1: Ignore GRANT in RX, check GRANT in TX. Independent of asserting REQUEST for RX. More...
|
|
uint8_t bKeepRequestIfNoGrant:1 |
| 0: Deassert REQUEST if GRANT was not given 1: Keep REQUEST asserted if no GRANT was given More...
|
|
} | cmdBleGenericRxConfig |
|
struct { |
uint8_t defaultPriority:1 |
| 0: Default low priority 1: Default high priority More...
|
|
uint8_t bAssertRequestForRx:1 |
| Default "request for RX" behaviour 0: Assert REQUEST for TX operations only 1: Assert REQUEST for both RX and TX operations. More...
|
|
uint8_t bIgnoreGrantInRx:1 |
| 0: Check GRANT in RX and TX 1: Ignore GRANT in RX, check GRANT in TX. Independent of asserting REQUEST for RX. More...
|
|
uint8_t bKeepRequestIfNoGrant:1 |
| 0: Deassert REQUEST if GRANT was not given 1: Keep REQUEST asserted if no GRANT was given More...
|
|
} | cmdBleTxTestConfig |
|