Data Fields
I2CCC26XX_Object Struct Reference

I2CCC26XX Object. More...

#include <I2CCC26XX.h>

Collaboration diagram for I2CCC26XX_Object:
Collaboration graph
[legend]

Data Fields

I2C_BASE_OBJECT SwiP_Struct swi
 
uint32_t bitRate
 
PIN_State pinState
 
PIN_Handle hPin
 
void * i2cPostFxn
 
Power_NotifyObj i2cPostObj
 

Detailed Description

I2CCC26XX Object.

The application must not access any member variables of this structure!

Field Documentation

§ swi

I2C_BASE_OBJECT SwiP_Struct I2CCC26XX_Object::swi

§ bitRate

uint32_t I2CCC26XX_Object::bitRate

§ pinState

PIN_State I2CCC26XX_Object::pinState

§ hPin

PIN_Handle I2CCC26XX_Object::hPin

§ i2cPostFxn

void* I2CCC26XX_Object::i2cPostFxn

§ i2cPostObj

Power_NotifyObj I2CCC26XX_Object::i2cPostObj

The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale