This module implements Real Time Localization System (RTLS) AoA post processing module.
More...
|
#define | MAX_SAMPLES_SINGLE_CHUNK 32 |
| Max number of samples reported in a single chunk when using RAW mode.
|
|
#define | REVERSE_SYNC_HANDLE 0x0FFF |
|
#define | SYNC_HANDLE_MASK 0x1000 |
|
|
rtlsStatus_e | RTLSCtrl_clInitAoa (aoaResultMode_e resultMode, uint8_t sampleCtrl, uint8_t numAnt, uint8_t *pAntPattern, uint16_t syncHandle) |
|
AoA_clSyncInfo_t * | RTLSCtrl_getClRes (uint16_t syncHnadle) |
|
void | RTLSCtrl_initAntConfig (void) |
|
rtlsStatus_e | RTLSCtrl_initAoa (uint8_t maxConnections, uint8_t sampleCtrl, uint8_t numAnt, uint8_t *pAntPattern, aoaResultMode_e resultMode) |
|
rtlsStatus_e | RTLSCtrl_initClResNode (uint16_t syncHandle) |
|
void | RTLSCtrl_postProcessAoa (rtlsAoaIqEvt_t *pEvt) |
| Called at the end of each connection event to extract I/Q samples. More...
|
|
void | RTLSCtrl_removeClAoaNode (uint16_t syncHandle) |
|
rtlsStatus_e | RTLSCtrl_verifyAntPattern (uint8_t sampleCtrl, uint8_t numAnt, uint8_t *pAntPattern) |
|
This module implements Real Time Localization System (RTLS) AoA post processing module.
§ RTLSCtrl_clInitAoa()
rtlsStatus_e RTLSCtrl_clInitAoa |
( |
aoaResultMode_e |
resultMode, |
|
|
uint8_t |
sampleCtrl, |
|
|
uint8_t |
numAnt, |
|
|
uint8_t * |
pAntPattern, |
|
|
uint16_t |
syncHandle |
|
) |
| |
RTLSCtrl_clInitAoa
Initialize connectionless AoA - has to be called before running AoA
- Parameters
-
resultMode | - AOA_MODE_ANGLE/AOA_MODE_PAIR_ANGLES/AOA_MODE_RAW |
sampleCtrl | - sample control configs: 0x01 = RAW RF, 0x00 = Filtered results (switching period omitted), bit 4,5 0x10 - ONLY_ANT_1, 0x20 - ONLY_ANT_2 |
numAnt | - Number of items in Antenna array |
pAntPattern | - Pointer to Antenna array |
syncHandle | - Handle identifying the periodic advertising train |
- Returns
- status - RTLS_AOA_CONFIG_NOT_SUPPORTED/RTLS_SUCCESS
§ RTLSCtrl_getClRes()
AoA_clSyncInfo_t* RTLSCtrl_getClRes |
( |
uint16_t |
syncHnadle | ) |
|
RTLSCtrl_getClRes
Find the CL AoA result node matching the given syncHandle
- Parameters
-
syncHandle | - Handle identifying the periodic advertising train |
- Returns
- pointer to AoA_clSyncInfo_t node if found. Else, NULL
§ RTLSCtrl_initAntConfig()
void RTLSCtrl_initAntConfig |
( |
void |
| ) |
|
RTLSCtrl_initAntConfig
Initialize the anternna configuration in the AoA control block
- Parameters
-
- Returns
- None
§ RTLSCtrl_initClResNode()
RTLSCtrl_initClResNode
Initialize new node for CL AoA angle mode and pair angle results
- Parameters
-
syncHandle | - Handle identifying the periodic advertising train |
- Returns
- RTLS_FAIL, RTLS_OUT_OF_MEMORY, RTLS_SUCCESS
§ RTLSCtrl_postProcessAoa()
void RTLSCtrl_postProcessAoa |
( |
rtlsAoaIqEvt_t * |
pEvt | ) |
|
Called at the end of each connection event to extract I/Q samples.
- Parameters
-
pEvt | - Pointer to IQ Event |
- Returns
- none
§ RTLSCtrl_removeClAoaNode()
void RTLSCtrl_removeClAoaNode |
( |
uint16_t |
syncHandle | ) |
|
RTLSCtrl_removeClAoaNode
Removes the node matching the given syncHandle
- Parameters
-
syncHandle | - Handle identifying the periodic advertising train |
- Returns
- None
§ RTLSCtrl_verifyAntPattern()
rtlsStatus_e RTLSCtrl_verifyAntPattern |
( |
uint8_t |
sampleCtrl, |
|
|
uint8_t |
numAnt, |
|
|
uint8_t * |
pAntPattern |
|
) |
| |
RTLSCtrl_verifyAntPattern
Check that a correct configuration was provided for the antenna pattern
- Parameters
-
sampleCtrl | - sample control configs: 0x01 = RAW RF, 0x00 = Filtered results (switching period omitted), bit 4,5 0x10 - ONLY_ANT_1, 0x20 - ONLY_ANT_2 |
numAnt | - Number of items in Antenna array |
pAntPattern | - Pointer to Antenna array |
- Returns
- status - RTLS_CONFIG_NOT_SUPPORTED/RTLS_SUCCESS