Z-Stack 3.4.0 to Z-Stack 3.5.0¶
This section will describe a way to migrate a project from Z-Stack 3.4.0 to a Z-Stack 3.5.0 project.
For this guide, zc_light_sink from Z-Stack 3.4.0 will be ported over to Z-Stack 3.5.0. The two releases have minor differences mostly pertaining to:
- Inclusion of the Common User Interface
- Improved NV driver
The recommended approach is to start with a Z-Stack 3.5.0 project that contains the same base application as the porting target project and merge any custom functionality.
Note
Although no Migration Guide was provided for Z-Stack 3.3.0 to Z-Stack 3.4.0, the only pertinent application changes are the addition of
POWER_TESTcases (see Example Application Power Test Definitions) and usingOsalPort_memcpyin place ofmemcpy.
- Choose a Z-Stack 3.5.0 example project that contains your target project’s base functionality. For reference and use in this example, zc_light_sink from C:\ti\simplelink_cc13x2_26x2_sdk_x_xx_xx_xx\examples\rtos\CC13x2 or CC26x2_LAUNCHXL\zstack is chosen as a starting point. 
- No changes are required for the Z-Stack 3.5.0 - zcl_samplelight_data.cfile unless clusters, attributes, or simple descriptors were added or altered in the Z-Stack 3.4.0 project.
- Small changes to - zcl_samplelight.hinclude application event changes and additional UI function definitions:- #include "cui.h" ... // Application Events #define SAMPLELIGHT_POLL_CONTROL_TIMEOUT_EVT 0x0001 #define SAMPLELIGHT_LEVEL_CTRL_EVT 0x0002 #define SAMPLEAPP_END_DEVICE_REJOIN_EVT 0x0004 #define SAMPLEAPP_DISCOVERY_TIMEOUT_EVT 0x0008 #define SAMPLEAPP_PROV_CONNECT_EVT 0x0080 #define SAMPLEAPP_PROV_DISCONNECT_EVT 0x0010 #define SAMPLEAPP_POLICY_UPDATE_EVT 0x0020 #define SAMPLEAPP_SYNC_ATTR_EVT 0x0040 ... /* * Function to toggle the light */ extern void zclSampleLight_UiActionToggleLight(const int32_t _itemEntry); /* * Function to discover switch devices to report state of the light */ extern void zclSampleLight_UiActionSwitchDiscovery(const int32_t _itemEntry); #ifdef USE_ZCL_SAMPLEAPP_UI #if defined (ENABLE_GREENPOWER_COMBO_BASIC) void zclSampleLight_setGPSinkCommissioningMode(const int32_t _itemEntry); #endif #endif 
The following items specifically concern zcl_samplelight.c:
- Common User Interface operation (identifiable by #ifdef USE_ZCL_SAMPLEAPP_UIand involving the new functions defined inzcl_samplelight.h) has replaced previous UI processes (including keys, LEDs, and UART).
- Addition of the Discovery clock, including extra functions and event handling.
- *_bdbGetZCLFrameCounter*is replaced with- *_getZCLFrameCounter*.
- New Match Descriptor Response and IEEE Address Response callbacks used for manual binds.
- zclSampleLight_dmmPausePolicyCbhas been added for- DMM_OAD.
- Updated parameter for zclSampleLight_setGPSinkCommissioningMode.
- If performing a field upgrade in which the NV memory is retained then
ZSTACK_NVOCMP_MIGRATIONmust be defined in the upgrade image to properly maintain NV item IDs while migrating from the old NVOCTP driver. If not using default NV item IDs from Z-Stack 3.4.0 then users must ensure that their legacy items are updated appropriately for Z-Stack 3.5.0, please refer tozgUpgradeNVDriverinside ofzglobals.cto accomplish this.
- Add any other Z-Stack 3.4.0 application changes to the Z-Stack 3.5.0 file if not pertaining to the items listed above.
Note
Difference comparison software is recommended for discerning all differences between software stacks.