Z-Stack 3.0.x to Z-Stack 3.1.0¶
This section will describe a way to migrate a project from Z-Stack 3.0.x to a Z-Stack 3.1.0 project.
For this guide, SampleLight from Z-Stack 3.0.x will be ported over to Z-Stack 3.1.0. The two releases are vastly divergent due to differences in both device and RTOS support, as is covered in CC253x to CC13x2 or CC26x2. The recommended approach is to start with a Z-Stack 3.1.0 project that contains the same base application as the porting target project and merge any custom functionality
- Choose a Z-Stack 3.1.0 example project that contains your target project’s base functionality. For reference and use in this example, zc_light from C:\ti\simplelink_zigbee_sdk_plugin_2_20_00_06\examples\rtos\CC13x2 or CC26x2_LAUNCHXL\zstack is chosen as a starting point. 
- No changes are required for the Z-Stack 3.1.0 - zcl_samplelight_data.cfile unless clusters, attributes, or simple descriptors were added or altered in the Z-Stack 3.0.x project.
- In - zcl_samplelight.h,- bdb_tlCommissioning.hhas been renamed- bdb_tl_commissioning.hand- /* * Application task entry point for the ZStack Sample Light Application */ extern void zclSampleLight_task(NVINTF_nvFuncts_t *pfnNV); - is used in place of - /* * Initialization for the task */ extern void zclSampleLight_Init( byte task_id ); /* * Event Process for the task */ extern UINT16 zclSampleLight_event_loop( byte task_id, UINT16 events ); 
- Do not copy the Z-Stack 3.0.x - OSAL_SampleLight.cfile and only make changes to the following lines of the 3.1.0- main.c- #include "zcl_samplelight.h" /* Kick off application */ zclSampleLight_task(&zstack_user0Cfg.nvFps); - if the task name has been changed inside of - zcl_samplelight.c
The following items specifically concern zcl_samplelight.c:
- Note the following changes due to the TI-RTOS implementation: - ICALL framework used to dispatch messages between Z-Stack and the application
- Semaphores used to post and pend during event callbacks
- Timer handling, i.e
 - Timer_setTimeout( LevelControlClkHandle, 100 ); Timer_start(&LevelControlClkStruct); - versus - osal_start_timerEx( zclSampleLight_TaskID, SAMPLELIGHT_LEVEL_CTRL_EVT, 100 );. Due to this and the reasons further provided below, all related code from Z-Stack 3.0.x should not be transferred to the Z-Stack 3.1.0 project.
- Key events are now handled locally in - zclSampleLight_processKeyinstead of- UI_MainStateMachinefrom- zcl_sampleapps_ui.c. A UART interface is preferred over LCD.
- main.ccalls the- zclSampleLight_taskfunction- void zclSampleLight_task(NVINTF_nvFuncts_t *pfnNV) { // Save and register the function pointers to the NV drivers pfnZdlNV = pfnNV; zclport_registerNV(pfnZdlNV, ZCL_PORT_SCENE_TABLE_NV_ID); // Initialize application zclSampleLight_initialization(); // No return from task process zclSampleLight_process_loop(); } - to initialize the application - static void zclSampleLight_initialization(void) { /* Initialize user clocks */ zclSampleLight_initializeClocks(); /* Initialize keys */ Board_Key_initialize(zclSampleLight_changeKeyCallback); /* Initialize the LEDS */ Board_Led_initialize(); // Register the current thread as an ICall dispatcher application // so that the application can send and receive messages. ICall_registerApp(&zclSampleLight_Entity, &sem); //Initialize stack zclSampleLight_Init(); } - which in-turn initializes the clocks, keys, LEDs, and ICall dispatcher before initializing the stack. This is compared with Z-Stack 3.0.x where all of the above was accomplished in - mainand- zclSampleLight_Init.
- zclSampleLight_Initregisters endpoints using- //Register Endpoint zclSampleLightEpDesc.endPoint = SAMPLELIGHT_ENDPOINT; zclSampleLightEpDesc.simpleDesc = &zclSampleLight_SimpleDesc; zclport_registerEndpoint(zclSampleLight_Entity, &zclSampleLightEpDesc); - instead of - // Register the Simple Descriptor for this application bdb_RegisterSimpleDescriptor( &zclSampleLight_SimpleDesc ); - and registers applications with - // Register the Application to receive the unprocessed Foundation command/response messages zclport_registerZclHandleExternal(zclSampleLight_ProcessIncomingMsg); - as compared to - // Register the Application to receive the unprocessed Foundation command/response messages zcl_registerForMsg( zclSampleLight_TaskID ); - Furthermore, bdb initialization parameters and ZDO callbacks are set up outside of - UI_Init- //Write the bdb initialization parameters zclSampleLight_initParameters(); //Setup ZDO callbacks SetupZStackCallbacks(); 
- Green Power is further expanded for endpoints, Application Events and Z-Stack messages: - gp_endpointInit(zclSampleLight_Entity);and- app_Green_Power_Initinside- zclSampleLight_Init
- In - zclSampleLight_process_loop- #if !defined (DISABLE_GREENPOWER_BASIC_PROXY) && (ZG_BUILD_RTR_TYPE) if(events & SAMPLEAPP_PROCESS_GP_DATA_SEND_EVT) { zcl_gpSendNotification(); events &= ~SAMPLEAPP_PROCESS_GP_DATA_SEND_EVT; } if(events & SAMPLEAPP_PROCESS_GP_EXPIRE_DUPLICATE_EVT) { gp_expireDuplicateFiltering(); events &= ~SAMPLEAPP_PROCESS_GP_EXPIRE_DUPLICATE_EVT; } #endif 
- In - zclSampleLight_processZStackMsgs:- #if !defined (DISABLE_GREENPOWER_BASIC_PROXY) && (ZG_BUILD_RTR_TYPE) case zstackmsg_CmdIDs_GP_DATA_IND: { zstackmsg_gpDataInd_t *pInd; pInd = (zstackmsg_gpDataInd_t*)pMsg; gp_processDataIndMsg( &(pInd->Req) ); } break; case zstackmsg_CmdIDs_GP_SECURITY_REQ: { zstackmsg_gpSecReq_t *pInd; pInd = (zstackmsg_gpSecReq_t*)pMsg; gp_processSecRecMsg( &(pInd->Req) ); } break; case zstackmsg_CmdIDs_GP_CHECK_ANNCE: { zstackmsg_gpCheckAnnounce_t *pInd; pInd = (zstackmsg_gpCheckAnnounce_t*)pMsg; gp_processCheckAnnceMsg( &(pInd->Req) ); } #endif 
 
- zclSampleLight_process_loopis used in place of- zclSampleLight_event_loopand uses ICall to receive messages instead of- SYS_EVENT_MSGevents and- osal_msg_receive- ICall_ServiceEnum stackid; ICall_EntityID dest; zstackmsg_genericReq_t *pMsg = NULL; /* Wait for response message */ if(ICall_wait(ICALL_TIMEOUT_FOREVER) == ICALL_ERRNO_SUCCESS) { /* Retrieve the response message */ if(ICall_fetchServiceMsg(&stackid, &dest, (void **)&pMsg) == ICALL_ERRNO_SUCCESS) { if( (stackid == ICALL_SERVICE_CLASS_ZSTACK) && (dest == zclSampleLight_Entity) ) { if(pMsg) { zclSampleLight_processZStackMsgs(pMsg); // Free any separately allocated memory Zstackapi_freeIndMsg(pMsg); } } if(pMsg) { ICall_freeMsg(pMsg); } } //**EVENT HANDLING NOT SHOWN** } 
- zclSampleLight_processZStackMsgsand- zclSampleLight_processAfIncomingMsgIndis used in place of- zclSampleLight_ProcessIncomingMsg- In - zclSampleLight_processZStackMsgs:- switch(pMsg->hdr.event) { //**OTHER CASES NOT SHOWN** case zstackmsg_CmdIDs_AF_INCOMING_MSG_IND: { // Process incoming data messages zstackmsg_afIncomingMsgInd_t *pInd; pInd = (zstackmsg_afIncomingMsgInd_t *)pMsg; zclSampleLight_processAfIncomingMsgInd( &(pInd->req) ); } break; } 
 
- Different APIs are used for BDB. For example, the - BDB_COMMISSIONING_FORMATIONcase inside of- zclSampleLight_ProcessCommissioningStatusis handled using- zstack_bdbStartCommissioningReq_t zstack_bdbStartCommissioningReq; //After formation, perform nwk steering again plus the remaining commissioning modes that has not been process yet zstack_bdbStartCommissioningReq.commissioning_mode = BDB_COMMISSIONING_MODE_NWK_STEERING | bdbCommissioningModeMsg->bdbRemainingCommissioningModes; Zstackapi_bdbStartCommissioningReq(zclSampleLight_Entity,&zstack_bdbStartCommissioningReq); - when it was previously - //After formation, perform nwk steering again plus the remaining commissioning modes that has not been process yet bdb_StartCommissioning(BDB_COMMISSIONING_MODE_NWK_STEERING | bdbCommissioningModeMsg->bdbRemainingCommissioningModes); 
- Structure type - zclIncomingMsg_thas been renamed- zclIncoming_t
- Add any other Z-Stack 3.0.x application changes to the Z-Stack 3.1.0 file if not pertaining to the items listed above 
Note
Difference comparison software is recommended for discerning all differences between software stacks.