TI BLE5-Stack API Documentation
2.01.04.00
|
LE CTE Connectionless IQ Report Event. More...
Data Fields | |
uint8 | BLEEventCode |
BLE Event Code. | |
uint8 | channelIndex |
index of channel | |
uint8 | cteType |
cte type | |
uint16 | eventCounter |
periodic adv event counter | |
osal_event_hdr_t | hdr |
osal event header | |
int8 * | iqSamples |
list of interleaved I/Q samples | |
uint16 | rssi |
current rssi | |
uint8 | rssiAntenna |
antenna ID | |
uint8 | sampleCount |
number of samples | |
uint8 | slotDuration |
sampling slot 1us or 2us | |
uint8 | status |
packet status (success or CRC error) | |
uint16 | syncHandle |
sync handle in periodic adv | |
LE CTE Connectionless IQ Report Event.