![]() |
![]() |
TI BLE5-Stack API Documentation
2.01.04.00
|
TOF Sync Structure. More...
Data Fields | |
TofSyncState_e | currentSyncState |
Current state of ToF Sync. | |
TofHandshakeState_e | handshakeState |
Holds the state of the Master<->Slave handshake (i.e if Master->Slave Slave->Master Master->Slave exchange was completed) | |
uint16_t | internalCtr |
Internal counter that counts how many ToF bursts (runs) we processed so far. | |
uint8_t | lastBuffFilled |
Holds the last buffer that was filled (in case ToF Security is using double buffer mode) | |
uint16_t | lastSharedCtr |
Last instance of shared counter as captured by the RTLS Passive. | |
uint16_t | numBuffSwitchRemaining |
Counts for the current ToF run, how many buffer switches are remaining until the run ends. | |
broadCast_t | tofBroadcast |
RF data. | |
TOF Sync Structure.