![]() |
![]() |
TI BLE5-Stack API Documentation
2.01.04.00
|
TOF Parameters Structure. More...
Data Fields | |
uint8_t | freqChangePeriod |
How often should we change freq? | |
uint8_t | mask |
Mask for the LFSR. | |
uint8_t | numFreq |
Number of frequencies in above list. | |
uint16_t | numSyncwordsPerBurst |
Number of bursts to be made (same as sync word length if using single buffer) | |
TOF_ApplicationCB | pfnTofApplicationCB |
Callback to application. | |
uint16_t * | pFrequencies |
Pointer to Frequencies. | |
uint8_t | postProcessLqiThresh |
LQI threshold used for onchip post processing. | |
uint16_t | postProcessMagnRatio |
Magnitude radio threshold used for onchip post processing. | |
uint8_t * | pRxBuf |
Pointer to Rx buffer. | |
ToF_Sample * | pT1RSSIBuf |
Pointer to T1|RSSI result buffer. | |
uint8_t * | pTxBuf |
Pointer to Tx buffer. | |
uint8_t | slaveLqiFilter |
Automatic filtering for ToF Slave role. | |
uint16_t | syncTimeout |
How long to wait for first sync word. | |
ToF_Role | tofRole |
Slave or master. | |
tofSecCfgPrms_t | tofSecurityParams |
TOF Security Configuration Paramaters. | |
TOF Parameters Structure.