![]() |
![]() |
TI BLE5-Stack API Documentation
2.01.04.00
|
Macros | |
#define | ATT_ERR_ATTR_NOT_FOUND 0x0a |
No attribute found within the given attribute handle range. | |
#define | ATT_ERR_ATTR_NOT_LONG 0x0b |
Attribute cannot be read or written using the Read Blob Request or Prepare Write Request. | |
#define | ATT_ERR_INSUFFICIENT_AUTHEN 0x05 |
The attribute requires authentication before it can be read or written. | |
#define | ATT_ERR_INSUFFICIENT_AUTHOR 0x08 |
The attribute requires an authorization before it can be read or written. | |
#define | ATT_ERR_INSUFFICIENT_ENCRYPT 0x0f |
The attribute requires encryption before it can be read or written. | |
#define | ATT_ERR_INSUFFICIENT_KEY_SIZE 0x0c |
The Encryption Key Size used for encrypting this link is insufficient. | |
#define | ATT_ERR_INSUFFICIENT_RESOURCES 0x11 |
Insufficient Resources to complete the request. | |
#define | ATT_ERR_INVALID_HANDLE 0x01 |
Attribute handle value given was not valid on this attribute server. | |
#define | ATT_ERR_INVALID_OFFSET 0x07 |
Offset specified was past the end of the attribute. | |
#define | ATT_ERR_INVALID_PDU 0x04 |
The attribute PDU was invalid. | |
#define | ATT_ERR_INVALID_VALUE 0x80 |
The attribute value is invalid for the operation. | |
#define | ATT_ERR_INVALID_VALUE_SIZE 0x0d |
The attribute value length is invalid for the operation. | |
#define | ATT_ERR_PREPARE_QUEUE_FULL 0x09 |
Too many prepare writes have been queued. | |
#define | ATT_ERR_READ_NOT_PERMITTED 0x02 |
Attribute cannot be read. | |
#define | ATT_ERR_UNLIKELY 0x0e |
The attribute request that was requested has encountered an error that was very unlikely, and therefore could not be completed as requested. | |
#define | ATT_ERR_UNSUPPORTED_GRP_TYPE 0x10 |
The attribute type is not a supported grouping attribute as defined by a higher layer specification. | |
#define | ATT_ERR_UNSUPPORTED_REQ 0x06 |
Attribute server doesn't support the request received from the attribute client. | |
#define | ATT_ERR_WRITE_NOT_PERMITTED 0x03 |
Attribute cannot be written. | |