Data Fields
SPICC26X2DMA_HWAttrs Struct Reference

SPICC26X2DMA Hardware attributes. More...

#include <SPICC26X2DMA.h>

Data Fields

uint32_t baseAddr
 SPI Peripheral's base address. More...
 
uint8_t intNum
 
uint8_t intPriority
 SPI CC26XXDMA Peripheral's interrupt priority. More...
 
uint32_t swiPriority
 SPI SWI priority. The higher the number, the higher the priority. The minimum is 0 and the maximum is 15 by default. The maximum can be reduced to save RAM by adding or modifying Swi.numPriorities in the kernel configuration file. More...
 
PowerCC26XX_Resource powerMngrId
 
uint16_t defaultTxBufValue
 
uint32_t rxChannelBitMask
 
uint32_t txChannelBitMask
 
PIN_Id mosiPin
 
PIN_Id misoPin
 
PIN_Id clkPin
 
PIN_Id csnPin
 
uint32_t minDmaTransferSize
 

Detailed Description

SPICC26X2DMA Hardware attributes.

These fields, with the exception of intPriority, are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For CC26xxWare these definitions are found in:

intPriority is the SPI peripheral's interrupt priority, as defined by the underlying OS. It is passed unmodified to the underlying OS's interrupt handler creation code, so you need to refer to the OS documentation for usage. For example, for SYS/BIOS applications, refer to the ti.sysbios.family.arm.m3.Hwi documentation for SYS/BIOS usage of interrupt priorities. If the driver uses the ti.dpl interface instead of making OS calls directly, then the HwiP port handles the interrupt priority in an OS specific way. In the case of the SYS/BIOS port, intPriority is passed unmodified to Hwi_create().

A sample structure is shown below:

const SPICC26X2DMA_HWAttrs SPICC26X2DMAobjects[] = {
{
.baseAddr = SSI0_BASE,
.intNum = INT_SPI0,
.intPriority = ~0,
.swiPriority = 0,
.powerMngrId = PERIPH_SPI0,
.defaultTxBufValue = 0,
.rxChannelBitMask = UDMA_CHAN_SPI0_RX,
.txChannelBitMask = UDMA_CHAN_SPI0_TX,
.mosiPin = CONFIG_SPI0_MISO,
.misoPin = CONFIG_SPI0_MOSI,
.clkPin = CONFIG_SPI0_CLK,
.csnPin = CONFIG_SPI0_CSN
},
{
.baseAddr = SSI1_BASE,
.intNum = INT_SPI1,
.intPriority = ~0,
.swiPriority = 0,
.powerMngrId = PERIPH_SPI1,
.defaultTxBufValue = 0,
.rxChannelBitMask = UDMA_CHAN_SPI1_RX,
.txChannelBitMask = UDMA_CHAN_SPI1_TX,
.mosiPin = CONFIG_SPI1_MISO,
.misoPin = CONFIG_SPI1_MOSI,
.clkPin = CONFIG_SPI1_CLK,
.csnPin = CONFIG_SPI1_CSN
},
};

Field Documentation

§ baseAddr

uint32_t SPICC26X2DMA_HWAttrs::baseAddr

SPI Peripheral's base address.

§ intNum

uint8_t SPICC26X2DMA_HWAttrs::intNum

SPI CC26XXDMA Peripheral's interrupt vector

§ intPriority

uint8_t SPICC26X2DMA_HWAttrs::intPriority

SPI CC26XXDMA Peripheral's interrupt priority.

The CC26xx uses three of the priority bits, meaning ~0 has the same effect as (7 << 5).

(7 << 5) will apply the lowest priority.

(1 << 5) will apply the highest priority.

Setting the priority to 0 is not supported by this driver.

HWI's with priority 0 ignore the HWI dispatcher to support zero-latency interrupts, thus invalidating the critical sections in this driver.

§ swiPriority

uint32_t SPICC26X2DMA_HWAttrs::swiPriority

SPI SWI priority. The higher the number, the higher the priority. The minimum is 0 and the maximum is 15 by default. The maximum can be reduced to save RAM by adding or modifying Swi.numPriorities in the kernel configuration file.

§ powerMngrId

PowerCC26XX_Resource SPICC26X2DMA_HWAttrs::powerMngrId

SPI Peripheral's power manager ID

§ defaultTxBufValue

uint16_t SPICC26X2DMA_HWAttrs::defaultTxBufValue

Default TX value if txBuf == NULL

§ rxChannelBitMask

uint32_t SPICC26X2DMA_HWAttrs::rxChannelBitMask

uDMA controlTable channel index

§ txChannelBitMask

uint32_t SPICC26X2DMA_HWAttrs::txChannelBitMask

uDMA controlTable channel index

§ mosiPin

PIN_Id SPICC26X2DMA_HWAttrs::mosiPin

SPI MOSI pin

§ misoPin

PIN_Id SPICC26X2DMA_HWAttrs::misoPin

SPI MISO pin

§ clkPin

PIN_Id SPICC26X2DMA_HWAttrs::clkPin

SPI CLK pin

§ csnPin

PIN_Id SPICC26X2DMA_HWAttrs::csnPin

SPI CSN pin

§ minDmaTransferSize

uint32_t SPICC26X2DMA_HWAttrs::minDmaTransferSize

Minimum transfer size for DMA based transfer


The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale