![]() |
![]() |
SDSPI Hardware attributes. More...
#include <SDSPI.h>
Data Fields | |
uint_least8_t | spiIndex |
uint16_t | spiCsGpioIndex |
SDSPI Hardware attributes.
The SDSPI_HWAttrs configuration structure contains the index of the SPI peripheral to be used for data transfers & the index of the GPIO Pin which will act as chip select. This driver uses this information to:
An example configuration structure could look as the following:
uint_least8_t SDSPI_HWAttrs::spiIndex |
uint16_t SDSPI_HWAttrs::spiCsGpioIndex |