Data Fields
PDMCC26XX_I2S_StreamNotification Struct Reference

A PDMCC26XX_I2S_StreamNotification data structure is used with PDMCC26XX_I2S_CallbackFxn(). Provides notification about available buffers and potential errors. More...

#include <PDMCC26XX_util.h>

Data Fields

void * arg
 
PDMCC26XX_I2S_Status status
 

Detailed Description

A PDMCC26XX_I2S_StreamNotification data structure is used with PDMCC26XX_I2S_CallbackFxn(). Provides notification about available buffers and potential errors.

Field Documentation

§ arg

void* PDMCC26XX_I2S_StreamNotification::arg

Argument to be passed to the callback function

§ status

PDMCC26XX_I2S_Status PDMCC26XX_I2S_StreamNotification::status

Status code set by PDMCC26XX_I2S driver


The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale