![]() |
![]() |
LED Object structure. More...
#include <LED.h>
Data Fields | |
uint32_t | pwmPeriod |
PWM_Handle | pwmHandle |
ClockP_Handle | clockHandle |
ClockP_Struct | clock |
LED_State | state |
LED_State | rawState |
LED_Type | ledType |
uint8_t | brightness |
uint_least8_t | gpioIndex |
uint16_t | togglePeriod |
uint16_t | blinkCount |
LED Object structure.
The application must not access any member variables of this structure!
uint32_t LED_Object::pwmPeriod |
pwmPeriod(us) of controlling PWM
PWM_Handle LED_Object::pwmHandle |
Used for PWM calls if PWM type LED
ClockP_Handle LED_Object::clockHandle |
Handle to clock used for blinking
ClockP_Struct LED_Object::clock |
Clock internal data
LED_State LED_Object::state |
Current State of LED
LED_State LED_Object::rawState |
rawState maintains actual state On or Off while blinking which is super state
LED_Type LED_Object::ledType |
may be either GPIO or PWM controlled
uint8_t LED_Object::brightness |
Varying min-max(0-100%) for PWM LED)
uint_least8_t LED_Object::gpioIndex |
Index into GPIO_PinConfig array
uint16_t LED_Object::togglePeriod |
Toggleperiod(ms), 0 for non-blinking LED This is half of blinkPeriod: two toggles is one blink
uint16_t LED_Object::blinkCount |
Blinkcount, 0 for non-blinking LED