Data Fields
AESECBCC26XX_Object Struct Reference

AESECBCC26XX Object. More...

#include <AESECBCC26XX.h>

Collaboration diagram for AESECBCC26XX_Object:
Collaboration graph
[legend]

Data Fields

bool isOpen
 
bool operationInProgress
 
bool operationCanceled
 
bool threadSafe
 
int_fast16_t returnStatus
 
AESECB_ReturnBehavior returnBehavior
 
AESECB_OperationType operationType
 
uint32_t semaphoreTimeout
 
AESECB_CallbackFxn callbackFxn
 
AESECB_Operationoperation
 

Detailed Description

AESECBCC26XX Object.

The application must not access any member variables of this structure!

Field Documentation

§ isOpen

bool AESECBCC26XX_Object::isOpen

§ operationInProgress

bool AESECBCC26XX_Object::operationInProgress

§ operationCanceled

bool AESECBCC26XX_Object::operationCanceled

§ threadSafe

bool AESECBCC26XX_Object::threadSafe

§ returnStatus

int_fast16_t AESECBCC26XX_Object::returnStatus

§ returnBehavior

AESECB_ReturnBehavior AESECBCC26XX_Object::returnBehavior

§ operationType

AESECB_OperationType AESECBCC26XX_Object::operationType

§ semaphoreTimeout

uint32_t AESECBCC26XX_Object::semaphoreTimeout

§ callbackFxn

AESECB_CallbackFxn AESECBCC26XX_Object::callbackFxn

§ operation

AESECB_Operation* AESECBCC26XX_Object::operation

The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale