Data Fields
AESCBCCC26XX_Object Struct Reference

AESCBCCC26XX Object. More...

#include <AESCBCCC26XX.h>

Collaboration diagram for AESCBCCC26XX_Object:
Collaboration graph
[legend]

Data Fields

bool isOpen
 
bool operationInProgress
 
bool operationCanceled
 
bool threadSafe
 
int_fast16_t returnStatus
 
AESCBC_ReturnBehavior returnBehavior
 
AESCBC_OperationType operationType
 
uint32_t semaphoreTimeout
 
AESCBC_CallbackFxn callbackFxn
 
AESCBC_Operationoperation
 
uint8_t iv [16]
 

Detailed Description

AESCBCCC26XX Object.

The application must not access any member variables of this structure!

Field Documentation

§ isOpen

bool AESCBCCC26XX_Object::isOpen

§ operationInProgress

bool AESCBCCC26XX_Object::operationInProgress

§ operationCanceled

bool AESCBCCC26XX_Object::operationCanceled

§ threadSafe

bool AESCBCCC26XX_Object::threadSafe

§ returnStatus

int_fast16_t AESCBCCC26XX_Object::returnStatus

§ returnBehavior

AESCBC_ReturnBehavior AESCBCCC26XX_Object::returnBehavior

§ operationType

AESCBC_OperationType AESCBCCC26XX_Object::operationType

§ semaphoreTimeout

uint32_t AESCBCCC26XX_Object::semaphoreTimeout

§ callbackFxn

AESCBC_CallbackFxn AESCBCCC26XX_Object::callbackFxn

§ operation

AESCBC_Operation* AESCBCCC26XX_Object::operation

§ iv

uint8_t AESCBCCC26XX_Object::iv[16]

The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale