![]() |
![]() |
PDM driver implementation for a CC26XX PDM controller.
============================================================================
The PDM header file should be included in an application as follows:
This driver is written to be able to perform continuous audio streaming of PDM data from a microphone. It also controls one DIO to be able to turn on power to the microphone.
This PDM driver performs two operations that requires processing
When producing 16kHz output, the driver is configured to process 256 bytes of PDM data provided by the I2S hardware module at a time, sampled at 1.024 Mbps. The PDM driver consequently receives such a buffer approximately every 2ms. A frame of PDMCC26XX_Params.retBufSizeInBytes PCM data bytes minus four metadata bytes is provided to the application after being filled by all or part of one or more 64 byte buffers of PCM data derived from the 256 bytes of PDM data. The resulting PCM frame provided to the application is a 16bit PCM signal sampled at 16kHz.
When providing 8kHz PCM output, the driver processes 512 bytes of PDM data at a time. At a sample rate of 1.024 Mbps, this yields a PDM buffer to process ever 4ms. These 512 bytes of PDM data are filtered and decimated to yield 64 bytes of PCM output.
The driver creates a separate task to run in.
The driver currently only samples on a single edge of the I2S clock.
Before using PDM on CC26XX:
While using PDM on CC26XX:
After PDM operation has ended:
The application is notified of errors via the registered callback function.
If the application fails to consume PCM buffers fast enough and the heap is full when driver tries to allocate a new buffer, the driver will drop all new incoming data until a buffer can be allocated to store it. Data is dropped one PCM data buffer at a time , even though it is streamed into the device and copied into the buffer in smaller chunks. This is done to keep the data expected in any buffer in sync with the sequence number of the buffer that keeps incrementing even when the buffer is dopped. The application may keep track of lost frames by comparing sequence numbers.
Hence, the PDM stream will never have a buffer overflow, but if the memory available in the heap is too low it may lose frames because because there is nowhere to put the incoming
If the heap frees up again and the PDM task runs, it will automatically resume normal operation again. The only application-observable difference is the incremented version number.
The application must permit the PDM task to run often enough that it can process a PDM buffer every 2ms on average. If the application requires a larger contiguous segment of processing time, the I2S hwi may run out of empty buffers to fill with new PDM data. When the I2S driver runs out of empty PDM buffers it will pop a buffer from the full buffer queue and overwrite its old data. The I2S driver notifies the PDM driver that it has dropped a PDM buffer. Once it runs again, the PDM driver will drop enough additional PCM samples such that the sequence numbers of the PCM buffers remain aligned with the data in the audio stream. The latency between when the PDM task was last serviced and when it must be serviced again to avoid losing data is specified by PDMCC26XX_Params::pdmBufferQueueDepth. This permitted latency increases by 2ms or 4ms for each increment of pdmBufferQueueDepth.
PDMCC26XX_open() returns NULL and rolls back all prior parts of the initialisation if any part of the initialisation fails. The following can cause PDMCC26XX_open() to fail:
PDMCC26XX_startStream() returns false if it fails. The following can cause PDMCC26XX_startStream() to fail:
PDMCC26XX_stopStream() returns false if it fails. The following can cause PDMCC26XX_stopStream() to fail:
The PDMCC26XX driver sets a power constraint while streaming to keep the device out of standby. When the stream has ended, the power constraint is released.
The following statements are valid:
The standard use case involves calling PDMCC26XX_open() once and calling PDMCC26XX_startStream() and PDMCC26XX_stopStream() to start and stop the stream as needed. PDMCC26XX_close() is called when the PDM driver will no longer be needed again. In order for the PDM driver task to run, the application pends on a semaphore that is posted in the PDMCC26XX_Params::callbackFxn. In this example, the application requests 128 buffers. In a real application, the process of pending on a semaphore, requesting a buffer, and freeing it would be repeated as often as required by the use case before stopping the stream.
By default, the PCM output of the driver has a sampling frequency of fs = 16kHz. There is an alternate signal processing chain that returns PCM output with fs = 8kHz. This example shows how to alter the standard use-case to set this up.
#include <ti/drivers/dpl/HwiP.h>
#include <ti/drivers/dpl/SemaphoreP.h>
#include <ti/drivers/PIN.h>
#include <ti/drivers/Power.h>
#include <ti/drivers/power/PowerCC26XX.h>
Go to the source code of this file.
Data Structures | |
struct | PDMCC26XX_metaData |
Metadata associated with an array of PCM data. More... | |
struct | PDMCC26XX_pcmBuffer |
PCM buffer pointed to in a PDMCC26XX_BufferRequest. More... | |
struct | PDMCC26XX_Config |
The PDMCC26XX_Config structure contains a set of pointers used to characterize the PDMCC26XX driver implementation. More... | |
struct | PDMCC26XX_HWAttrs |
PDMCC26XX Hardware attributes. More... | |
struct | PDMCC26XX_StreamNotification |
A PDMCC26XX_StreamNotification data structure is used with PDMCC26XX_CallbackFxn(). Provides notification about available buffers and potential errors. More... | |
struct | PDMCC26XX_BufferRequest |
A PDMCC26XX_BufferRequest data structure is used with PDMCC26XX_requestBuffer(). More... | |
struct | PDMCC26XX_Params |
PDMCC26XX Parameters are used to with the PDMCC26XX_open() call. Default values for these parameters are set using PDMCC26XX_Params_init(). More... | |
struct | PDMCC26XX_Object |
PDMCC26XX Object. More... | |
Macros | |
#define | PDM_TASK_STACK_SIZE 850 |
#define | PCM_SAMPLE_SIZE 16 |
#define | PCM_COMPRESSION_RATE 4 |
#define | MINIMUM_PDM_BUFFER_QUEUE_DEPTH 3 |
#define | PCM_METADATA_SIZE sizeof(PDMCC26XX_metaData) |
Typedefs | |
typedef void *(* | PDMCC26XX_MallocFxn) (size_t memSize) |
PDMCC26XX_MallocFxn is a function pointer for the malloc function to be used by the driver. More... | |
typedef void(* | PDMCC26XX_FreeFxn) (void *ptr, size_t memSize) |
PDMCC26XX_FreeFxn is a function pointer for the free function to be used by the driver. This is needed for memory clean up, if something goes wrong. More... | |
typedef bool(* | PDMCC26XX_Pdm2PcmFxn) (const void *pdmInBuffer, uint32_t *decimationState, const int32_t *biquadCoefficients, int16_t *pcmOutBuffer) |
Function that converts PDM input buffer to PCM output. More... | |
typedef PDMCC26XX_Config * | PDMCC26XX_Handle |
A handle that is returned from a PDMCC26XX_open() call. More... | |
typedef void(* | PDMCC26XX_CallbackFxn) (PDMCC26XX_Handle handle, PDMCC26XX_StreamNotification *streamNotification) |
The definition of a callback function used when buffers are ready. More... | |
Enumerations | |
enum | PDMCC26XX_Status { PDMCC26XX_STREAM_IDLE, PDMCC26XX_STREAM_BLOCK_READY, PDMCC26XX_STREAM_BLOCK_READY_BUT_PDM_OVERFLOW, PDMCC26XX_STREAM_ERROR, PDMCC26XX_STREAM_STOPPING, PDMCC26XX_STREAM_STOPPED, PDMCC26XX_STREAM_FAILED_TO_STOP } |
Status codes that are set by the PDM driver. More... | |
enum | PDMCC26XX_PcmSampleRate { PDMCC26XX_PCM_SAMPLE_RATE_16K = 0, PDMCC26XX_PCM_SAMPLE_RATE_8K } |
PCM output sample rates supported by the driver. More... | |
enum | PDMCC26XX_Gain { PDMCC26XX_GAIN_24 = 1318, PDMCC26XX_GAIN_18 = 660, PDMCC26XX_GAIN_12 = 331, PDMCC26XX_GAIN_6 = 166, PDMCC26XX_GAIN_0 = 83, PDMCC26XX_GAIN_END } |
Predefined gain settings. More... | |
Functions | |
void | PDMCC26XX_init (PDMCC26XX_Handle handle) |
PDM CC26XX initialization. More... | |
PDMCC26XX_Handle | PDMCC26XX_open (PDMCC26XX_Params *params) |
Function to initialize the CC26XX PDM peripheral specified by the particular handle. The parameter specifies which mode the PDM will operate. More... | |
void | PDMCC26XX_close (PDMCC26XX_Handle handle) |
Function to close a given CC26XX PDM peripheral specified by the PDM handle. More... | |
bool | PDMCC26XX_startStream (PDMCC26XX_Handle handle) |
Function to start streaming PDM data. More... | |
bool | PDMCC26XX_stopStream (PDMCC26XX_Handle handle) |
Function to stop streaming PDM data. More... | |
bool | PDMCC26XX_requestBuffer (PDMCC26XX_Handle handle, PDMCC26XX_BufferRequest *bufferRequest) |
Function for requesting buffer. More... | |
void | PDMCC26XX_Params_init (PDMCC26XX_Params *params) |
Variables | |
const PDMCC26XX_Config | PDMCC26XX_config [] |
#define PDM_TASK_STACK_SIZE 850 |
Defines TI-RTOS stack size allocation. It is a conservative estimate. Change this to save a few bytes of RAM on stack allocation. The stack usage is independent of the PCM return buffer size specified by the application. When using logging, increase this value. This value is also dependent on the malloc and free function implementations provided by the application as both are called from PDM task context.
#define PCM_SAMPLE_SIZE 16 |
Uncompressed PCM sample size in bits
#define PCM_COMPRESSION_RATE 4 |
Compression rate if compression is enabled
#define MINIMUM_PDM_BUFFER_QUEUE_DEPTH 3 |
Minimum number of PDM buffers required by the driver to safely use the I2S module
#define PCM_METADATA_SIZE sizeof(PDMCC26XX_metaData) |
PCM data metadata size. When a buffer is requested there will be metadata prepended. In other words the pointer returned points to the metadata header. Depending on the mode, this contains different information. The first byte is always an 8-bit sequence number.
typedef void*(* PDMCC26XX_MallocFxn) (size_t memSize) |
PDMCC26XX_MallocFxn is a function pointer for the malloc function to be used by the driver.
typedef void(* PDMCC26XX_FreeFxn) (void *ptr, size_t memSize) |
PDMCC26XX_FreeFxn is a function pointer for the free function to be used by the driver. This is needed for memory clean up, if something goes wrong.
typedef bool(* PDMCC26XX_Pdm2PcmFxn) (const void *pdmInBuffer, uint32_t *decimationState, const int32_t *biquadCoefficients, int16_t *pcmOutBuffer) |
Function that converts PDM input buffer to PCM output.
pdmInBuffer | Input PDM buffer |
decimationState | CIC decimator state |
biquadCoefficients | Coefficient table for the n-stage biquad IIR filter |
pcmOutBuffer | Output PCM buffer |
typedef PDMCC26XX_Config* PDMCC26XX_Handle |
A handle that is returned from a PDMCC26XX_open() call.
typedef void(* PDMCC26XX_CallbackFxn) (PDMCC26XX_Handle handle, PDMCC26XX_StreamNotification *streamNotification) |
The definition of a callback function used when buffers are ready.
PDMCC26XX_Handle | PDMCC26XX_Handle |
enum PDMCC26XX_Status |
Status codes that are set by the PDM driver.
enum PDMCC26XX_Gain |
Predefined gain settings.
Gain is controlled by modifying the first coefficient of the PDM filter. Use these defines to set the correct gain setting in the default filter. This setting does not affect any non-default filters! All values are in dB. Default prefilter stages will add 12dB gain. PDM2PCM algorithm returns false if any of the samples decimated goes above 2^16 - 1, i.e. the sample clipped during decimation. This information can be used for automatic gain control.
Enumerator | |
---|---|
PDMCC26XX_GAIN_24 | 24dB gain |
PDMCC26XX_GAIN_18 | 18dB gain |
PDMCC26XX_GAIN_12 | 12dB gain. Default |
PDMCC26XX_GAIN_6 | 6dB gain |
PDMCC26XX_GAIN_0 | 0dB gain |
PDMCC26XX_GAIN_END | Internal use only |
void PDMCC26XX_init | ( | PDMCC26XX_Handle | handle | ) |
PDM CC26XX initialization.
PDMCC26XX_Handle PDMCC26XX_open | ( | PDMCC26XX_Params * | params | ) |
Function to initialize the CC26XX PDM peripheral specified by the particular handle. The parameter specifies which mode the PDM will operate.
The function will set a dependency on the PDM module, which in turn powers up the module and enables the clock. IOs are also allocated, however the PDM driver will not begin streaming audio until PDMCC26XX_startStream() is called.
params | Pointer to a parameter block. Will use default parameters if NULL |
void PDMCC26XX_close | ( | PDMCC26XX_Handle | handle | ) |
Function to close a given CC26XX PDM peripheral specified by the PDM handle.
Posts an event that shuts down the I2S hardware, frees all memory used by the driver on the heap, releases the pins back to the PIN driver, and releases the dependency on the corresponding power domain.
handle | A PDMCC26XX_Handle returned from PDMCC26XX_open() |
bool PDMCC26XX_startStream | ( | PDMCC26XX_Handle | handle | ) |
Function to start streaming PDM data.
Posts an event that tells the I2S hardware to start streaming and the PDM task to start processing incoming data.
handle | A PDM handle returned from PDMCC26XX_open() |
bool PDMCC26XX_stopStream | ( | PDMCC26XX_Handle | handle | ) |
Function to stop streaming PDM data.
Blocks while the I2S module shuts down gracefully. Subsequently posts an event to let the PDM task process any remaining data.
handle | A PDM handle returned from PDMCC26XX_open() |
bool PDMCC26XX_requestBuffer | ( | PDMCC26XX_Handle | handle, |
PDMCC26XX_BufferRequest * | bufferRequest | ||
) |
Function for requesting buffer.
PDMCC26XX_requestBuffer returns immediately even if no buffer is available. The caller is notified through events each time a buffer is available. However, more than one buffer may be available. Hence, the caller should request even without notification if the caller is ready to process.
handle | A PDM handle returned from PDMCC26XX_open() |
*bufferRequest | Pointer to PDMCC26XX_BufferRequest struct |
void PDMCC26XX_Params_init | ( | PDMCC26XX_Params * | params | ) |
const PDMCC26XX_Config PDMCC26XX_config[] |
PDMCC26XX_Config struct defined in the board file