![]() |
![]() |
TI-15.4 Stack API
3.20.00.10
|
#include <api_mac.h>
Data Fields | |
ApiMac_status_t | status |
ApiMac_scantype_t | scanType |
uint8_t | channelPage |
uint8_t | phyId |
uint8_t | unscannedChannels [APIMAC_154G_CHANNEL_BITMAP_SIZ] |
uint8_t | resultListSize |
union { | |
uint8_t * pEnergyDetect | |
ApiMac_panDesc_t * pPanDescriptor | |
} | result |
MAC_MLME_SCAN_CNF type
ApiMac_status_t _apimac_mlmescancnf::status |
status of the scan request
ApiMac_scantype_t _apimac_mlmescancnf::scanType |
The type of scan requested
uint8_t _apimac_mlmescancnf::channelPage |
The channel page of the scan
uint8_t _apimac_mlmescancnf::phyId |
PHY ID corresponding to the PHY descriptor used during scan
uint8_t _apimac_mlmescancnf::unscannedChannels[APIMAC_154G_CHANNEL_BITMAP_SIZ] |
Bit mask of channels that were not scanned
uint8_t _apimac_mlmescancnf::resultListSize |
The number of PAN descriptors returned in the results list
uint8_t* _apimac_mlmescancnf::pEnergyDetect |
The list of energy measurements, one for each channel scanned
ApiMac_panDesc_t* _apimac_mlmescancnf::pPanDescriptor |
The list of PAN descriptors, one for each beacon found
union { ... } _apimac_mlmescancnf::result |
Depending on the scanType the results are in this union