![]() |
![]() |
TI-15.4 Stack API
3.20.00.10
|
#include <api_mac.h>
Data Fields | |
uint8_t | numPendShortAddr |
uint16_t * | pShortAddrList |
uint8_t | numPendExtAddr |
uint8_t * | pExtAddrList |
uint8_t | sduLength |
uint8_t * | pSdu |
MAC Beacon data type
uint8_t _apimac_beacondata::numPendShortAddr |
The number of pending short addresses
uint16_t* _apimac_beacondata::pShortAddrList |
The list of device short addresses for which the sender of the beacon has data
uint8_t _apimac_beacondata::numPendExtAddr |
The number of pending extended addresses
uint8_t* _apimac_beacondata::pExtAddrList |
The list of device short addresses for which the sender of the beacon has data
uint8_t _apimac_beacondata::sduLength |
The number of bytes in the beacon payload of the beacon frame
uint8_t* _apimac_beacondata::pSdu |
The beacon payload