#include <rf_prop_cmd.h>
|
uint16_t | nRxOk |
| Number of packets that have been received with payload, CRC OK and not ignored. More...
|
|
uint16_t | nRxNok |
| Number of packets that have been received with CRC error. More...
|
|
uint8_t | nRxIgnored |
| Number of packets that have been received with CRC OK and ignored due to address mismatch. More...
|
|
uint8_t | nRxStopped |
| Number of packets not received due to illegal length or address mismatch with pktConf.filterOp = 1. More...
|
|
uint8_t | nRxBufFull |
| Number of packets that have been received and discarded due to lack of buffer space. More...
|
|
int8_t | lastRssi |
| RSSI of last received packet. More...
|
|
ratmr_t | timeStamp |
| Time stamp of last received packet. More...
|
|
§ nRxOk
uint16_t rfc_propRxOutput_s::nRxOk |
Number of packets that have been received with payload, CRC OK and not ignored.
§ nRxNok
uint16_t rfc_propRxOutput_s::nRxNok |
Number of packets that have been received with CRC error.
§ nRxIgnored
uint8_t rfc_propRxOutput_s::nRxIgnored |
Number of packets that have been received with CRC OK and ignored due to address mismatch.
§ nRxStopped
uint8_t rfc_propRxOutput_s::nRxStopped |
Number of packets not received due to illegal length or address mismatch with pktConf.filterOp = 1.
§ nRxBufFull
uint8_t rfc_propRxOutput_s::nRxBufFull |
Number of packets that have been received and discarded due to lack of buffer space.
§ lastRssi
int8_t rfc_propRxOutput_s::lastRssi |
RSSI of last received packet.
§ timeStamp
ratmr_t rfc_propRxOutput_s::timeStamp |
Time stamp of last received packet.
The documentation for this struct was generated from the following file: