![]() |
![]() |
rflib
|
Set New Synthesizer Frequency without Recalibration. More...
#include <rf_common_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number 0x0013. More... | |
uint16_t | frequency |
The frequency in MHz to tune to. More... | |
uint16_t | fractFreq |
Fractional part of the frequency to tune to. More... | |
Set New Synthesizer Frequency without Recalibration.
uint16_t rfc_CMD_MODIFY_FS_s::commandNo |
The command ID number 0x0013.
uint16_t rfc_CMD_MODIFY_FS_s::frequency |
The frequency in MHz to tune to.
uint16_t rfc_CMD_MODIFY_FS_s::fractFreq |
Fractional part of the frequency to tune to.