CC26xx Driver Library
prcm.c File Reference
#include "prcm.h"

Macros

#define PRCM_PERIPH_INDEX(a)   (((a) >> 8) & 0xf)
 
#define PRCM_PERIPH_MASKBIT(a)   (0x00000001 << ((a) & 0x1f))
 

Functions

void PRCMInfClockConfigureSet (uint32_t ui32ClkDiv, uint32_t ui32PowerMode)
 Configure the infrastructure clock. More...
 
uint32_t PRCMInfClockConfigureGet (uint32_t ui32PowerMode)
 Use this function to get the infrastructure clock configuration. More...
 
void PRCMAudioClockConfigSet (uint32_t ui32ClkConfig, uint32_t ui32SampleRate)
 Configure the audio clock generation. More...
 
void PRCMAudioClockConfigSetOverride (uint32_t ui32ClkConfig, uint32_t ui32MstDiv, uint32_t ui32BitDiv, uint32_t ui32WordDiv)
 Configure the audio clock generation with manual setting of clock divider. More...
 
void PRCMAudioClockConfigOverride (uint8_t ui8SamplingEdge, uint8_t ui8WCLKPhase, uint32_t ui32MstDiv, uint32_t ui32BitDiv, uint32_t ui32WordDiv)
 Configure the audio clocks for I2S module. More...
 
void PRCMAudioClockInternalSource (void)
 Configure the audio clocks to be internally generated. More...
 
void PRCMAudioClockExternalSource (void)
 Configure the audio clocks to be externally generated. More...
 
void PRCMPowerDomainOn (uint32_t ui32Domains)
 Turn power on in power domains in the MCU domain. More...
 
void PRCMPowerDomainOff (uint32_t ui32Domains)
 Turn off a specific power domain. More...
 
void PRCMPeripheralRunEnable (uint32_t ui32Peripheral)
 Enables a peripheral in Run mode. More...
 
void PRCMPeripheralRunDisable (uint32_t ui32Peripheral)
 Disables a peripheral in Run mode. More...
 
void PRCMPeripheralSleepEnable (uint32_t ui32Peripheral)
 Enables a peripheral in sleep mode. More...
 
void PRCMPeripheralSleepDisable (uint32_t ui32Peripheral)
 Disables a peripheral in sleep mode. More...
 
void PRCMPeripheralDeepSleepEnable (uint32_t ui32Peripheral)
 Enables a peripheral in deep-sleep mode. More...
 
void PRCMPeripheralDeepSleepDisable (uint32_t ui32Peripheral)
 Disables a peripheral in deep-sleep mode. More...
 
uint32_t PRCMPowerDomainsAllOff (uint32_t ui32Domains)
 Get the status for a specific power domain. More...
 
uint32_t PRCMPowerDomainsAllOn (uint32_t ui32Domains)
 Get the status for a specific power domain. More...
 
void PRCMDeepSleep (void)
 Put the processor into deep-sleep mode. More...
 

Variables

static const uint32_t g_pui32RCGCRegs []
 
static const uint32_t g_pui32SCGCRegs []
 
static const uint32_t g_pui32DCGCRegs []
 

Macro Definition Documentation

Variable Documentation

const uint32_t g_pui32DCGCRegs[]
static
Initial value:
=
{
PRCM_O_GPTCLKGDS ,
PRCM_O_SSICLKGDS ,
PRCM_O_UARTCLKGDS ,
PRCM_O_I2CCLKGDS ,
PRCM_O_SECDMACLKGDS ,
PRCM_O_GPIOCLKGDS ,
PRCM_O_I2SCLKGDS
}

Referenced by PRCMPeripheralDeepSleepDisable(), and PRCMPeripheralDeepSleepEnable().

const uint32_t g_pui32RCGCRegs[]
static
Initial value:
=
{
PRCM_O_GPTCLKGR ,
PRCM_O_SSICLKGR ,
PRCM_O_UARTCLKGR ,
PRCM_O_I2CCLKGR ,
PRCM_O_SECDMACLKGR ,
PRCM_O_GPIOCLKGR ,
PRCM_O_I2SCLKGR
}

Referenced by PRCMPeripheralRunDisable(), and PRCMPeripheralRunEnable().

const uint32_t g_pui32SCGCRegs[]
static
Initial value:
=
{
PRCM_O_GPTCLKGS ,
PRCM_O_SSICLKGS ,
PRCM_O_UARTCLKGS ,
PRCM_O_I2CCLKGS ,
PRCM_O_SECDMACLKGS ,
PRCM_O_GPIOCLKGS ,
PRCM_O_I2SCLKGS
}

Referenced by PRCMPeripheralSleepDisable(), and PRCMPeripheralSleepEnable().