TI BLE5-Stack API Documentation
2.01.03.00
|
Macros | |
#define | OAD_EXT_CTRL_BLK_RSP_NOTIF 0x12 |
#define | OAD_EXT_CTRL_CANCEL_OAD 0x05 |
#define | OAD_EXT_CTRL_DISABLE_BLK_NOTIF 0x06 |
#define | OAD_EXT_CTRL_ENABLE_IMG 0x04 |
#define | OAD_EXT_CTRL_ERASE_BONDS 0x13 |
#define | OAD_EXT_CTRL_GET_BLK_SZ 0x01 |
#define | OAD_EXT_CTRL_GET_DEV_TYPE 0x10 |
#define | OAD_EXT_CTRL_GET_IMG_INFO 0x11 |
#define | OAD_EXT_CTRL_GET_IMG_STAT 0x08 |
#define | OAD_EXT_CTRL_GET_PROF_VER 0x09 |
#define | OAD_EXT_CTRL_GET_SW_VER 0x07 |
#define | OAD_EXT_CTRL_IMG_CNT 0x02 |
#define | OAD_EXT_CTRL_START_OAD 0x03 |
#define OAD_EXT_CTRL_BLK_RSP_NOTIF 0x12 |
Send block request external control command op-code This command is used to send a block request notification to the peer device
#define OAD_EXT_CTRL_CANCEL_OAD 0x05 |
Cancel OAD external control command op-code This command is used to cancel the OAD process
#define OAD_EXT_CTRL_DISABLE_BLK_NOTIF 0x06 |
Disable block notification external control command op-code This command is used to disable the image block request notifications
#define OAD_EXT_CTRL_ENABLE_IMG 0x04 |
Enable image external control command op-code This command is used to enable an image after download, instructing the target to prepare the image to run and then reboot
#define OAD_EXT_CTRL_ERASE_BONDS 0x13 |
Erase bonds external control command op-code This command is used to erase all BLE bonding info on the device
#define OAD_EXT_CTRL_GET_BLK_SZ 0x01 |
Get Block Size external control command op-code This command is used by a peer to determine what is the largest block size the target can support
#define OAD_EXT_CTRL_GET_DEV_TYPE 0x10 |
Get device type external control command op-code This command is used to query type of the device the profile is running on
#define OAD_EXT_CTRL_GET_IMG_INFO 0x11 |
Get image info external control command op-code This command is used to get the image info structure corresponding to the the image asked for
#define OAD_EXT_CTRL_GET_IMG_STAT 0x08 |
Get status external control command op-code This command is used to query the status of the OAD process.
#define OAD_EXT_CTRL_GET_PROF_VER 0x09 |
Get profile version external control command op-code This command is used to query the version of the OAD profile
#define OAD_EXT_CTRL_GET_SW_VER 0x07 |
Get software version external control command op-code This command is used to query the OAD target device for its software version
#define OAD_EXT_CTRL_IMG_CNT 0x02 |
Get image count external control command op-code This command is used by a peer to instruct the target that multiple images are to be downloaded during this session
#define OAD_EXT_CTRL_START_OAD 0x03 |
Start OAD external control command op-code This command is used to tell the target device that the configuration stage has completed and it is time to start sending block requests