Terms and Acronyms

General Terms and Acronyms

BDB
Base Device Behavior
CCA
Customer Configuration area, see CCFG
CCFG
Customer Configuration Area, contains lock-bits on flash page 31 and the Customer Configuration Table (.ccfg)
CCS
Code Composer Studio
DMM
Dynamic Multi-protocol Manager
GCC
GNU Compiler Collection
IAR
IAR Systems
ICALL
Indirect Call
IEEE 802.15.4
The Institue of Electrical and Electronics Engineers 802.15.4 protocol specifies the physical and medium access layers for wireless Personal Area Networks targeted at low power, low data rate applications
MCU
Microcontroller Unit
OAD
Over the Air Download
OTA
Over the Air
OTA Client
A device capable of downloading an image from an OTA Server using the OTA cluster
OTA Server
A device capable of hosting an image for download by an OTA Client using the OTA cluster
PAN
Personal Area Network
RCFG
TI-RTOS in ROM Configuration Table
RTOS
Real Time Operating System
RTSC
Real Time Software Components
ROM
Read-only Memory
SC
Sensor Controller
SCS
Sensor Controller Studio
SNV
Simple Non-Volatile storage
SoC
System on Chip - processor core and radio are integrated on same device
cjtag
2-wire debug interface
jtag
4-wire debug interface

TI-RTOS Terms and Acronyms

HWI
Hardware Interrupts
A TI-RTOS hardware interrupt.
Idle Task
A TI-RTOS default task that is executes when no other higher priority thread needs to run.
RCFG
TI-RTOS in ROM configuration table.
ROV
Runtime Object View
A TI-RTOS kernel plugin for CCS and IAR to view a target’s instrumentation data.
RTC
Real-Time Clock
An accurate computer clock which keeps track of the current time.
RTOS
Real Time Operating System
An operating system intended to serve applications with real-time requirements.
SWI
Software Interrupts
A TI-RTOS software interrupt.
TI-RTOS
Texas Instruments Real Time Operating System
An RTOS developed by TI for TI microcontrollers.
Zero-Latency Interrupts
An interrupt that will not be routed through the TI-RTOS kernel’s Hwi dispatcher. For more information, see the Hwi module documentation in the TI-RTOS Kernel API Reference .

Sensor Controller Terms and Acronyms

SC
Sensor Controller
A dedicated 16-bit CPU core on CC13xx and CC26xx devices, located in the auxiliary (AUX) power/clock domain. It can perform simple background tasks autonomously and independently of the System CPU and the MCU domain power states.
SCS
Sensor Controller Studio
A stand-alone IDE used to write, test and debug code for the Sensor Controller.

Over-the-Air Download (OAD) Terms and Acronyms

BIM
Boot Image Manager
A bootloader that runs after the device’s ROM startup code. The BIM is responsible for analyzing the image header of all images and determining the most suitable image to run. Once the BIM has found the proper image, it will jump to it’s program entry.
CRC
Cyclic Redundancy Check
An error-detecting code used to check the integrity of blocks of data.
ECDSA
Elliptic Curve Digital Signature Algorithm
A variant of the Digital Signature Algorithm (DSA) which uses elliptic curve cryptography.
Factory Image
The factory image is a “golden” image that resides in external flash as a fail-safe mechanism.
HIB
Halt In Boot
A mechanism in CC26xx and CC13xx devices to ensure that the external emulator can take control of the device before it executes any application code.
OAD
Over-the-Air Download
The process of performing a device firmware update over the air.
OAD Target
The device whose firmware is being upgraded over the air. This is assumed to be a CC26xx or CC13xx device running the TI protocol-specific transport for OAD.
OAD Distributor
The device responsible for accepting an OAD enabled image from the compiler and transferring it over the air to the OAD Target.