![]() |
![]() |
UART2CC26X2 Object. More...
#include <UART2CC26X2.h>
Data Fields | |
struct { | |
bool opened:1 | |
UART2_Mode readMode | |
UART2_Mode writeMode | |
UART2_ReadReturnMode readReturnMode:1 | |
bool txEnabled:1 | |
} | state |
HwiP_Struct | hwi |
uint32_t | baudRate |
UART2_DataLen | dataLength |
UART2_StopBits | stopBits |
UART2_Parity | parityType |
int32_t | rxStatus |
int32_t | txStatus |
void * | userArg |
UDMACC26XX_Handle | udmaHandle |
volatile tDMAControlTable * | rxDmaEntry |
volatile tDMAControlTable * | txDmaEntry |
unsigned char * | readBuf |
size_t | readSize |
uint32_t | nReadTransfers |
size_t | readCount |
size_t | rxSize |
size_t | bytesRead |
SemaphoreP_Struct | readSem |
UART2_Callback | readCallback |
const unsigned char * | writeBuf |
size_t | writeSize |
uint32_t | nWriteTransfers |
size_t | writeCount |
size_t | txSize |
size_t | bytesWritten |
SemaphoreP_Struct | writeSem |
UART2_Callback | writeCallback |
PIN_State | pinState |
PIN_Handle | hPin |
Power_NotifyObj | postNotify |
unsigned int | powerMgrId |
UART2CC26X2 Object.
The application must not access any member variables of this structure!
bool UART2CC26X2_Object::opened |
UART2_Mode UART2CC26X2_Object::readMode |
UART2_Mode UART2CC26X2_Object::writeMode |
UART2_ReadReturnMode UART2CC26X2_Object::readReturnMode |
bool UART2CC26X2_Object::txEnabled |
struct { ... } UART2CC26X2_Object::state |
HwiP_Struct UART2CC26X2_Object::hwi |
uint32_t UART2CC26X2_Object::baudRate |
UART2_DataLen UART2CC26X2_Object::dataLength |
UART2_StopBits UART2CC26X2_Object::stopBits |
UART2_Parity UART2CC26X2_Object::parityType |
int32_t UART2CC26X2_Object::rxStatus |
int32_t UART2CC26X2_Object::txStatus |
void* UART2CC26X2_Object::userArg |
UDMACC26XX_Handle UART2CC26X2_Object::udmaHandle |
volatile tDMAControlTable* UART2CC26X2_Object::rxDmaEntry |
volatile tDMAControlTable* UART2CC26X2_Object::txDmaEntry |
unsigned char* UART2CC26X2_Object::readBuf |
size_t UART2CC26X2_Object::readSize |
uint32_t UART2CC26X2_Object::nReadTransfers |
size_t UART2CC26X2_Object::readCount |
size_t UART2CC26X2_Object::rxSize |
size_t UART2CC26X2_Object::bytesRead |
SemaphoreP_Struct UART2CC26X2_Object::readSem |
UART2_Callback UART2CC26X2_Object::readCallback |
const unsigned char* UART2CC26X2_Object::writeBuf |
size_t UART2CC26X2_Object::writeSize |
uint32_t UART2CC26X2_Object::nWriteTransfers |
size_t UART2CC26X2_Object::writeCount |
size_t UART2CC26X2_Object::txSize |
size_t UART2CC26X2_Object::bytesWritten |
SemaphoreP_Struct UART2CC26X2_Object::writeSem |
UART2_Callback UART2CC26X2_Object::writeCallback |
PIN_State UART2CC26X2_Object::pinState |
PIN_Handle UART2CC26X2_Object::hPin |
Power_NotifyObj UART2CC26X2_Object::postNotify |
unsigned int UART2CC26X2_Object::powerMgrId |