#include <TimerCC26XX.h>
Data Fields | |
GPTimerCC26XX_Handle | gptHandle |
SemaphoreP_Struct | semStruct |
SemaphoreP_Handle | semHandle |
Timer_CallBackFxn | callBack |
Timer_Mode | mode |
uint32_t | period |
bool | isRunning |
bool | isOpen |
The application must not access any member variables of this structure!
GPTimerCC26XX_Handle TimerCC26XX_Object::gptHandle |
SemaphoreP_Struct TimerCC26XX_Object::semStruct |
SemaphoreP_Handle TimerCC26XX_Object::semHandle |
Timer_CallBackFxn TimerCC26XX_Object::callBack |
Timer_Mode TimerCC26XX_Object::mode |
uint32_t TimerCC26XX_Object::period |
bool TimerCC26XX_Object::isRunning |
bool TimerCC26XX_Object::isOpen |