Data Fields
AESCCMCC26XX_Object Struct Reference

AESCCMCC26XX Object. More...

#include <AESCCMCC26XX.h>

Collaboration diagram for AESCCMCC26XX_Object:
Collaboration graph
[legend]

Data Fields

bool isOpen
 
bool operationInProgress
 
bool operationCanceled
 
int_fast16_t returnStatus
 
AESCCM_ReturnBehavior returnBehavior
 
AESCCM_OperationType operationType
 
uint32_t semaphoreTimeout
 
AESCCM_CallbackFxn callbackFxn
 
AESCCM_Operationoperation
 

Detailed Description

AESCCMCC26XX Object.

The application must not access any member variables of this structure!

Field Documentation

§ isOpen

bool AESCCMCC26XX_Object::isOpen

§ operationInProgress

bool AESCCMCC26XX_Object::operationInProgress

§ operationCanceled

bool AESCCMCC26XX_Object::operationCanceled

§ returnStatus

int_fast16_t AESCCMCC26XX_Object::returnStatus

§ returnBehavior

AESCCM_ReturnBehavior AESCCMCC26XX_Object::returnBehavior

§ operationType

AESCCM_OperationType AESCCMCC26XX_Object::operationType

§ semaphoreTimeout

uint32_t AESCCMCC26XX_Object::semaphoreTimeout

§ callbackFxn

AESCCM_CallbackFxn AESCCMCC26XX_Object::callbackFxn

§ operation

AESCCM_Operation* AESCCMCC26XX_Object::operation

The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale