![]() |
![]() |
Analog to Digital Conversion Buffer (ADCBuf) Input Driver.
The ADCBuf driver allows you to sample and convert analog signals at a specified frequency. The resulting samples are placed in a buffer provided by the application. The driver can either take N
samples once or continuously sample by double-buffering and providing a callback to process each finished buffer.
This documentation provides a basic usage summary and a set of examples in the form of commented code fragments. Detailed descriptions of the APIs are provided in subsequent sections.
Refer to the Driver's Configuration section for driver configuration information.
#include <stdint.h>
Go to the source code of this file.
Data Structures | |
struct | ADCBuf_Conversion |
Defines a conversion to be used with ADCBuf_convert(). More... | |
struct | ADCBuf_Params |
ADCBuf parameters used with ADCBuf_open(). More... | |
struct | ADCBuf_FxnTable |
The definition of an ADCBuf function table that contains the required set of functions to control a specific ADC driver implementation. More... | |
struct | ADCBuf_Config_ |
ADC driver's custom configuration structure. More... | |
Macros | |
#define | ADCBuf_CMD_RESERVED (32) |
#define | ADCBuf_STATUS_RESERVED (-32) |
#define | ADCBuf_STATUS_SUCCESS (0) |
Success status code returned by: ADCBuf_control() More... | |
#define | ADCBuf_STATUS_ERROR (-1) |
Generic error status code returned by ADCBuf_control(). More... | |
#define | ADCBuf_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by ADCBuf_control() for undefined command codes. More... | |
#define | ADCBuf_STATUS_UNSUPPORTED (-3) |
An error status code returned if the function is not supported by a particular driver implementation. More... | |
Typedefs | |
typedef struct ADCBuf_Config_ * | ADCBuf_Handle |
A handle that is returned from an ADCBuf_open() call. More... | |
typedef void(* | ADCBuf_Callback) (ADCBuf_Handle handle, ADCBuf_Conversion *conversion, void *completedADCBuffer, uint32_t completedChannel, int_fast16_t status) |
The definition of a callback function. More... | |
typedef struct ADCBuf_Config_ | ADCBuf_Config |
ADC driver's custom configuration structure. More... | |
Enumerations | |
enum | ADCBuf_Recurrence_Mode { ADCBuf_RECURRENCE_MODE_ONE_SHOT, ADCBuf_RECURRENCE_MODE_CONTINUOUS } |
Recurrence behavior of a ADCBuf_Conversion specified in the ADCBuf_Params. More... | |
enum | ADCBuf_Return_Mode { ADCBuf_RETURN_MODE_BLOCKING, ADCBuf_RETURN_MODE_CALLBACK } |
Return behavior for ADCBuf_convert() specified in the ADCBuf_Params. More... | |
Functions | |
void | ADCBuf_close (ADCBuf_Handle handle) |
Function to close an ADCBuf driver instance. More... | |
int_fast16_t | ADCBuf_control (ADCBuf_Handle handle, uint_fast16_t cmd, void *cmdArg) |
Function performs implementation specific features on a driver instance. More... | |
void | ADCBuf_init (void) |
Function to initialize the ADCBuf driver. More... | |
void | ADCBuf_Params_init (ADCBuf_Params *params) |
Initialize an ADCBuf_Params structure to its default values. More... | |
ADCBuf_Handle | ADCBuf_open (uint_least8_t index, ADCBuf_Params *params) |
This function opens a given ADCBuf peripheral. More... | |
int_fast16_t | ADCBuf_convert (ADCBuf_Handle handle, ADCBuf_Conversion conversions[], uint_fast8_t channelCount) |
Starts ADCBuf conversions on one or more channels. More... | |
int_fast16_t | ADCBuf_convertCancel (ADCBuf_Handle handle) |
Cancels all ADCBuf conversions in progress. More... | |
uint_fast8_t | ADCBuf_getResolution (ADCBuf_Handle handle) |
Returns the resolution in bits of the specified ADCBuf instance. More... | |
int_fast16_t | ADCBuf_adjustRawValues (ADCBuf_Handle handle, void *sampleBuf, uint_fast16_t sampleCount, uint32_t adcChan) |
Adjust a raw ADC output buffer. The function does the adjustment in-place. More... | |
int_fast16_t | ADCBuf_convertAdjustedToMicroVolts (ADCBuf_Handle handle, uint32_t adcChan, void *adjustedSampleBuffer, uint32_t outputMicroVoltBuffer[], uint_fast16_t sampleCount) |
Convert an adjusted ADC output buffer to microvolts. More... | |
typedef struct ADCBuf_Config_* ADCBuf_Handle |
A handle that is returned from an ADCBuf_open() call.
typedef void(* ADCBuf_Callback) (ADCBuf_Handle handle, ADCBuf_Conversion *conversion, void *completedADCBuffer, uint32_t completedChannel, int_fast16_t status) |
The definition of a callback function.
When operating in ADCBuf_RETURN_MODE_CALLBACK, the callback function is called when an ADCBuf_Conversion completes. The application is responsible for declaring a ADCBuf_Callback and providing a pointer in ADCBuf_Params.callbackFxn.
[out] | handle | ADCBuf_Handle used with the initial call to ADCBuf_convert() |
[out] | conversion | Pointer to the ADCBuf_Conversion structure used with the initial call to ADCBuf_convert(). This structure also contains the custom argument specified by conversion.arg . |
[out] | completedADCBuffer | Pointer to a buffer containing conversion.samplesRequestedCount ADC samples. |
[out] | completedChannel | ADCBuf channel the samples were performed on. |
typedef struct ADCBuf_Config_ ADCBuf_Config |
ADC driver's custom configuration structure.
Recurrence behavior of a ADCBuf_Conversion specified in the ADCBuf_Params.
This enumeration defines the recurrence mode of a ADCBuf_Conversion. After a call to ADCBuf_convert(), ADCBuf_Conversion may either be done once or reoccur.
Enumerator | |
---|---|
ADCBuf_RECURRENCE_MODE_ONE_SHOT | When operating in ADCBuf_RECURRENCE_MODE_ONE_SHOT, calls to ADCBuf_convert() will pend on a semaphore until ADCBuf_Conversion.samplesRequestedCount samples are completed or after a duration of ADCBuf_Params.blockingTimeout.
|
ADCBuf_RECURRENCE_MODE_CONTINUOUS | When operating in ADCBuf_RECURRENCE_MODE_CONTINUOUS, calls to ADCBuf_convert() will return immediately. The driver will continuously perform ADCBuf_Conversion.samplesRequestedCount samples and call the ADCBuf_Callback function when completed. The driver will automatically alternate between ADCBuf_Conversion.sampleBuffer and ADCBuf_Conversion.sampleBufferTwo. A ADCBuf_RECURRENCE_MODE_CONTINUOUS conversion can only be terminated using ADCBuf_convertCancel().
|
enum ADCBuf_Return_Mode |
Return behavior for ADCBuf_convert() specified in the ADCBuf_Params.
This enumeration defines the return behavior for ADCBuf_convert(). A call to ADCBuf_convert() may either block or return immediately.
Enumerator | |
---|---|
ADCBuf_RETURN_MODE_BLOCKING | When operating in ADCBuf_RETURN_MODE_BLOCKING, calls to ADCBuf_convert() will pend on a semaphore until ADCBuf_Conversion.samplesRequestedCount samples are completed or after a duration of ADCBuf_Params.blockingTimeout.
|
ADCBuf_RETURN_MODE_CALLBACK | When operating in ADCBuf_RETURN_MODE_CALLBACK, calls to ADCBuf_convert() will return immediately. When ADCBuf_Conversion.samplesRequestedCount samples are completed, the ADCBuf_Params.callbackFxn function is called.
|
void ADCBuf_close | ( | ADCBuf_Handle | handle | ) |
Function to close an ADCBuf driver instance.
[in] | handle | An ADCBuf_Handle returned from ADCBuf_open() |
int_fast16_t ADCBuf_control | ( | ADCBuf_Handle | handle, |
uint_fast16_t | cmd, | ||
void * | cmdArg | ||
) |
Function performs implementation specific features on a driver instance.
[in] | handle | An ADCBuf_Handle returned from ADCBuf_open() |
[in] | cmd | A command value defined by the device specific implementation |
[in] | cmdArg | An optional R/W (read/write) argument that is accompanied with cmd |
ADCBuf_STATUS_SUCCESS | The call was successful. |
ADCBuf_STATUS_UNDEFINEDCMD | The cmd value is not supported by the device specific implementation. |
void ADCBuf_init | ( | void | ) |
Function to initialize the ADCBuf driver.
This function must also be called before any other ADCBuf driver APIs.
void ADCBuf_Params_init | ( | ADCBuf_Params * | params | ) |
Initialize an ADCBuf_Params structure to its default values.
[in] | params | A pointer to ADCBuf_Params structure for initialization |
Default values are:
ADCBuf_Handle ADCBuf_open | ( | uint_least8_t | index, |
ADCBuf_Params * | params | ||
) |
This function opens a given ADCBuf peripheral.
[in] | index | Index in the ADCBuf_Config [] array. |
[in] | params | Pointer to an initialized ADCBuf_Params structure. If NULL, the default ADCBuf_Params values are used. |
int_fast16_t ADCBuf_convert | ( | ADCBuf_Handle | handle, |
ADCBuf_Conversion | conversions[], | ||
uint_fast8_t | channelCount | ||
) |
Starts ADCBuf conversions on one or more channels.
[in] | handle | An ADCBuf handle returned from ADCBuf_open() |
[in] | conversions | A pointer to an array of ADCBuf_Conversion structures. |
[in] | channelCount | The number of channels to convert on in this call. Should be the length of the conversions array. Depending on the device, multiple simultaneous conversions may not be supported. See device specific implementation. |
ADCBuf_STATUS_SUCCESS | The conversion was successful. |
ADCBuf_STATUS_ERROR | The conversion failed. |
int_fast16_t ADCBuf_convertCancel | ( | ADCBuf_Handle | handle | ) |
Cancels all ADCBuf conversions in progress.
[in] | handle | An ADCBuf_Handle returned from ADCBuf_open() |
ADCBuf_STATUS_SUCCESS | The cancel was successful. |
ADCBuf_STATUS_ERROR | The cancel failed. |
uint_fast8_t ADCBuf_getResolution | ( | ADCBuf_Handle | handle | ) |
Returns the resolution in bits of the specified ADCBuf instance.
[in] | handle | An ADCBuf_Handle returned from ADCBuf_open(). |
int_fast16_t ADCBuf_adjustRawValues | ( | ADCBuf_Handle | handle, |
void * | sampleBuf, | ||
uint_fast16_t | sampleCount, | ||
uint32_t | adcChan | ||
) |
Adjust a raw ADC output buffer. The function does the adjustment in-place.
[in] | handle | An ADCBuf_Handle returned from ADCBuf_open(). |
[in,out] | sampleBuf | A buffer full of raw sample values. |
[in] | sampleCount | The number of samples to adjust. |
[in] | adcChan | The channel the buffer was sampled on. |
ADCBuf_STATUS_SUCCESS | The operation was successful. sampleBuf contains valid values. |
ADCBuf_STATUS_ERROR | if an error occurred. |
ADCBuf_STATUS_UNSUPPORTED | The function is not supported by the device specific implementation. |
int_fast16_t ADCBuf_convertAdjustedToMicroVolts | ( | ADCBuf_Handle | handle, |
uint32_t | adcChan, | ||
void * | adjustedSampleBuffer, | ||
uint32_t | outputMicroVoltBuffer[], | ||
uint_fast16_t | sampleCount | ||
) |
Convert an adjusted ADC output buffer to microvolts.
[in] | handle | An ADCBuf_Handle returned from ADCBuf_open() |
[in] | adcChan | The ADC channel the samples were performed on. |
[in] | adjustedSampleBuffer | A buffer full of adjusted samples. |
[in,out] | outputMicroVoltBuffer | The output buffer. |
[in] | sampleCount | The number of samples to convert. |
ADCBuf_STATUS_SUCCESS | The operation was successful. outputMicroVoltBuffer contains valid values. |
ADCBuf_STATUS_ERROR | The operation failed. |
adjustedSampleBuffer
.