TI-15.4 Stack API
3.20.00.10
|
#include <api_mac.h>
Data Fields | |
uint32_t | firstChCentrFreq |
uint16_t | numChannels |
uint32_t | channelSpacing |
uint8_t | fskModScheme |
uint16_t | symbolRate |
uint8_t | fskModIndex |
uint8_t | ccaType |
Generic PHY Descriptor. We are using this structure for both Channel Page 9 and Channel Page 10.
uint32_t _apimac_mrfskphydesc::firstChCentrFreq |
First Channel Center frequency
uint16_t _apimac_mrfskphydesc::numChannels |
Number of channels defined for the particular PHY mode
uint32_t _apimac_mrfskphydesc::channelSpacing |
Distance between Adjacent center channel frequencies
uint8_t _apimac_mrfskphydesc::fskModScheme |
2-FSK/2-GFSK/4-FSK/4-GFSK
uint16_t _apimac_mrfskphydesc::symbolRate |
Symbol rate selection
uint8_t _apimac_mrfskphydesc::fskModIndex |
Modulation index as a value encoded in MR-FSK Generic PHY Descriptor IE (IEEE802.15.4g section 5.2.4.20c).
2FSK MI = 0.25 + Modulation Index * 0.05
4FSK MI is a third of 2FSK MI
uint8_t _apimac_mrfskphydesc::ccaType |
Channel clearance algorithm selection