rflib
|
IEEE 802.15.4 Transmit Command. More...
#include <rf_ieee_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number 0x2C01. More... | |
uint16_t | status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More... | |
rfc_radioOp_t * | pNextOp |
Pointer to the next operation to run after this operation is done. More... | |
ratmr_t | startTime |
Absolute or relative start time (depending on the value of startTrigger ) More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | startTrigger |
Identification of the trigger that starts the operation. More... | |
struct { | |
uint8_t rule:4 | |
Condition for running next command: Rule for how to proceed. More... | |
uint8_t nSkip:4 | |
Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More... | |
} | condition |
struct { | |
uint8_t bIncludePhyHdr:1 | |
0: Find PHY header automatically 1: Insert PHY header from the buffer More... | |
uint8_t bIncludeCrc:1 | |
0: Append automatically calculated CRC 1: Insert FCS (CRC) from the buffer More... | |
uint8_t __pad0__:1 | |
uint8_t payloadLenMsb:5 | |
Most significant bits of payload length. Should only be non-zero to create long non-standard packets for test purposes. More... | |
} | txOpt |
uint8_t | payloadLen |
Number of bytes in the payload. More... | |
uint8_t * | pPayload |
Pointer to payload buffer of size payloadLen More... | |
ratmr_t | timeStamp |
Time stamp of transmitted frame. More... | |
IEEE 802.15.4 Transmit Command.
uint16_t rfc_CMD_IEEE_TX_s::commandNo |
The command ID number 0x2C01.
uint16_t rfc_CMD_IEEE_TX_s::status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.
rfc_radioOp_t* rfc_CMD_IEEE_TX_s::pNextOp |
Pointer to the next operation to run after this operation is done.
ratmr_t rfc_CMD_IEEE_TX_s::startTime |
Absolute or relative start time (depending on the value of startTrigger
)
uint8_t rfc_CMD_IEEE_TX_s::triggerType |
The type of trigger.
uint8_t rfc_CMD_IEEE_TX_s::bEnaCmd |
0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger
uint8_t rfc_CMD_IEEE_TX_s::triggerNo |
The trigger number of the CMD_TRIGGER command that triggers this action.
uint8_t rfc_CMD_IEEE_TX_s::pastTrig |
0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible
struct { ... } rfc_CMD_IEEE_TX_s::startTrigger |
Identification of the trigger that starts the operation.
uint8_t rfc_CMD_IEEE_TX_s::rule |
Condition for running next command: Rule for how to proceed.
uint8_t rfc_CMD_IEEE_TX_s::nSkip |
Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...
struct { ... } rfc_CMD_IEEE_TX_s::condition |
uint8_t rfc_CMD_IEEE_TX_s::bIncludePhyHdr |
0: Find PHY header automatically
1: Insert PHY header from the buffer
uint8_t rfc_CMD_IEEE_TX_s::bIncludeCrc |
0: Append automatically calculated CRC
1: Insert FCS (CRC) from the buffer
uint8_t rfc_CMD_IEEE_TX_s::__pad0__ |
uint8_t rfc_CMD_IEEE_TX_s::payloadLenMsb |
Most significant bits of payload length. Should only be non-zero to create long non-standard packets for test purposes.
struct { ... } rfc_CMD_IEEE_TX_s::txOpt |
uint8_t rfc_CMD_IEEE_TX_s::payloadLen |
Number of bytes in the payload.
uint8_t* rfc_CMD_IEEE_TX_s::pPayload |
Pointer to payload buffer of size payloadLen
ratmr_t rfc_CMD_IEEE_TX_s::timeStamp |
Time stamp of transmitted frame.