![]() |
![]() |
TI BLE5-Stack API Documentation
2.01.03.00
|
LE CTE Antenna Information Event RTLSSRV_ANTENNA_INFORMATION_EVT. More...
Data Fields | |
uint8_t | maxCteLen |
maximum cte length supported by the controller | |
uint8_t | maxNumOfAntennas |
maximum number of antennas supported by the controller | |
uint8_t | maxSwitchPatternLen |
maximum size of switch pattern supported by the controller | |
uint8_t | sampleRates |
sample rates supported by the controller | |
LE CTE Antenna Information Event RTLSSRV_ANTENNA_INFORMATION_EVT.