Data Fields
TimerCC26XX_Object Struct Reference

TimerCC26XX_Object. More...

#include <TimerCC26XX.h>

Collaboration diagram for TimerCC26XX_Object:
Collaboration graph
[legend]

Data Fields

GPTimerCC26XX_Handle gptHandle
 
SemaphoreP_Struct semStruct
 
SemaphoreP_Handle semHandle
 
Timer_CallBackFxn callBack
 
Timer_Mode mode
 
uint32_t period
 
bool isRunning
 
bool isOpen
 

Detailed Description

TimerCC26XX_Object.

The application must not access any member variables of this structure!

Field Documentation

§ gptHandle

GPTimerCC26XX_Handle TimerCC26XX_Object::gptHandle

§ semStruct

SemaphoreP_Struct TimerCC26XX_Object::semStruct

§ semHandle

SemaphoreP_Handle TimerCC26XX_Object::semHandle

§ callBack

Timer_CallBackFxn TimerCC26XX_Object::callBack

§ mode

Timer_Mode TimerCC26XX_Object::mode

§ period

uint32_t TimerCC26XX_Object::period

§ isRunning

bool TimerCC26XX_Object::isRunning

§ isOpen

bool TimerCC26XX_Object::isOpen

The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale