TI-15.4 Stack API
3.10.00.33
|
#include <api_mac.h>
Data Fields | |
ApiMac_sAddr_t | srcAddr |
uint16_t | srcPanId |
bool | noRsp |
MAC_MLME_POLL_IND type
ApiMac_sAddr_t _apimac_mlmepollind::srcAddr |
Address of the device sending the data request
uint16_t _apimac_mlmepollind::srcPanId |
Pan ID of the device sending the data request
bool _apimac_mlmepollind::noRsp |
indication that no MAC_McpsDataReq() is required. It is set when MAC_MLME_POLL_IND is generated, to simply indicate that a received data request frame was acked with pending bit cleared.