![]() |
![]() |
|
TI BLE5-Stack API Documentation
2.01.02.00
|
Event for advertising report. More...
Data Fields | |
| uint8_t | addr [B_ADDR_LEN] |
| Address of the advertising device. | |
| GAP_Addr_Types_t | addrType |
| Public, random, public ID, random ID, or anonymous. | |
| uint8_t | advSid |
| SID (0x00-0x0f) of the advertising PDU. 0xFF means no ADI field in the PDU. | |
| uint16_t | dataLen |
| Length of the data. | |
| uint8_t | directAddr [B_ADDR_LEN] |
| TargetA address. | |
| GAP_Addr_Types_t | directAddrType |
| Type of TargetA address in the directed advertising PDU. | |
| uint8_t | evtType |
| uint8_t * | pData |
| Pointer to advertising or scan response data. | |
| uint16_t | periodicAdvInt |
| Periodic advertising interval. 0 means no periodic advertising. | |
| GapScan_ScannedPhy_t | primPhy |
| PHY of the primary advertising channel. | |
| int8_t | rssi |
| -127 dBm <= RSSI <= 20 dBm | |
| GapScan_ScannedPhy_t | secPhy |
| PHY of the secondary advertising channel. | |
| int8_t | txPower |
| -127 dBm <= TX power <= 126 dBm | |
Event for advertising report.
| uint8_t evtType |
Bits 0 to 4 indicate connectable, scannable, directed, scan response, and legacy respectively